WSTK Sensors Plugin
Functions |
|
EmberStatus
|
emberAfPluginWstkSensorsGetSample (uint32_t *rhData, int32_t *tData) |
|
Reads a sample of the temperature and relative humidity values from the WSTK Si7013 sensors.
More...
|
|
Detailed Description
See
wstk-sensors.h
for source code.
Function Documentation
EmberStatus
emberAfPluginWstkSensorsGetSample
|
( | uint32_t * |
rhData,
|
| int32_t * |
tData
|
||
| ) |
Reads a sample of the temperature and relative humidity values from the WSTK Si7013 sensors.
- Parameters
-
rhDataA pointer to a 32-bit unsigned integer where the relative humidity sample is written. tDataA pointer to a 32-bit signed integer where the temperature is written. Temperature is sampled in "millicelsius".
- Returns
- An EmberStatus value of EMBER_SUCCESS if the relative humidity and temperature sample were successfully read from the Si7013 sensors. Otherwise, an EmberStatus value of EMBER_ERR_FATAL .