Memory Buffer
Macros |
|
| #define | EMBER_NULL_BUFFER |
|
A special
EmberBuffer
ID indicating that no memory is currently allocated.
More...
|
|
Handlers |
|
| void | emberMarkApplicationBuffersHandler (void) |
|
This handler is invoked by the memory buffers system garbage collector and allows the application to properly mark the application-defined
EmberBuffer
variables.
More...
|
|
APIs |
|
| EmberBuffer | emberAllocateBuffer (uint16_t dataSizeInBytes) |
|
Dynamically allocates memory.
More...
|
|
| void | emberMarkBuffer ( EmberBuffer *buffer) |
|
Prevents the garbage collector from reclaiming the memory associated with the passed
EmberBuffer
. The application should call this API within the
emberMarkApplicationBuffersHandler()
stack handler for each
EmberBuffer
object.
More...
|
|
| uint8_t * | emberGetBufferPointer ( EmberBuffer buffer) |
|
Returns a pointer to the memory segment corresponding to the passed
EmberBuffer
buffer. Notice that the garbage collector can move memory segments to defragment the available memory. As result, the application should always use this API to obtain an updated pointer prior to accessing the memory.
More...
|
|
| uint16_t | emberGetBufferLength ( EmberBuffer buffer) |
|
Returns the length in bytes of the passed
EmberBuffer
buffer.
More...
|
|
| uint16_t | emberGetAvailableBufferMemory (void) |
|
An API that returns the available memory at the buffer manager in bytes.
More...
|
|
Detailed Description
See
memory-buffer.h
for source code.
Macro Definition Documentation
| #define EMBER_NULL_BUFFER |
A special EmberBuffer ID indicating that no memory is currently allocated.
Definition at line
19
of file
memory-buffer.h
.
Function Documentation
| EmberBuffer emberAllocateBuffer | ( | uint16_t |
dataSizeInBytes
|
) |
Dynamically allocates memory.
- Parameters
-
dataSizeInBytesThe size in bytes of the memory to be allocated.
- Returns
- An EmberBuffer value of EMBER_NULL_BUFFER if the memory management system could not allocate the requested memory, or any other EmberBuffer value indicating that the requested memory was successfully allocated. The allocated memory can easily be freed by assigning an EmberBuffer variable to EMBER_NULL_BUFFER. The memory will be freed by the garbage collector during the next emberTick() call.
| uint16_t emberGetAvailableBufferMemory | ( | void |
|
) |
An API that returns the available memory at the buffer manager in bytes.
- Returns
- The number of available bytes.
| uint16_t emberGetBufferLength | ( | EmberBuffer |
buffer
|
) |
Returns the length in bytes of the passed EmberBuffer buffer.
- Parameters
-
bufferA pointer to the EmberBuffer buffer for which the corresponding length in bytes should be returned.
- Returns
- The length in bytes of a memory segment corresponding to the passed EmberBuffer buffer.
| uint8_t* emberGetBufferPointer | ( | EmberBuffer |
buffer
|
) |
Returns a pointer to the memory segment corresponding to the passed EmberBuffer buffer. Notice that the garbage collector can move memory segments to defragment the available memory. As result, the application should always use this API to obtain an updated pointer prior to accessing the memory.
- Parameters
-
bufferA pointer to the EmberBuffer buffer for which the corresponding memory pointer should be returned.
- Returns
- A NULL pointer if the passed EmberBuffer value is EMBER_NULL_BUFFER . Otherwise, a pointer to the corresponding memory segment.
| void emberMarkApplicationBuffersHandler | ( | void |
|
) |
This handler is invoked by the memory buffers system garbage collector and allows the application to properly mark the application-defined EmberBuffer variables.
| void emberMarkBuffer | ( | EmberBuffer * |
buffer
|
) |
Prevents the garbage collector from reclaiming the memory associated with the passed EmberBuffer . The application should call this API within the emberMarkApplicationBuffersHandler() stack handler for each EmberBuffer object.
- Parameters
-
bufferA pointer to the EmberBuffer buffer to be marked.