A struct containing all of the function pointers needed to implement secure element Authenticated Encryption with Additional Data operations.
PSA Crypto API implementations should populate instances of the table as appropriate upon startup.
If one of the functions is not implemented, it should be set to NULL.
Public Functions#
MBEDTLS_PRIVATE(p_encrypt)
Function that performs the AEAD encrypt operation.
MBEDTLS_PRIVATE(p_decrypt)
Function that performs the AEAD decrypt operation.
Public Function Documentation#
MBEDTLS_PRIVATE#
psa_drv_se_aead_encrypt_t psa_drv_se_aead_t::MBEDTLS_PRIVATE (p_encrypt )
Function that performs the AEAD encrypt operation.
Parameters
N/A |
Definition at line
802
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h
MBEDTLS_PRIVATE#
psa_drv_se_aead_decrypt_t psa_drv_se_aead_t::MBEDTLS_PRIVATE (p_decrypt )
Function that performs the AEAD decrypt operation.
Parameters
N/A |
Definition at line
804
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h