Builtin keys on devices with Secure Engine#
These key ID values belong to the builtin range of PSA, and allow access to the keys which respectively are and can be preprovisioned in Secure Engine devices.
Refer to Built-in keys or AN1311 for more information on the usage of builtin keys through PSA Crypto.
Macros#
Vendor Key ID for the built-in application identity key on Vault High devices.
Vendor Key ID for the built-in SE identity key on Vault High devices.
Vendor Key ID for the Secure Boot verifying key provisioned to the Secure Engine.
Vendor Key ID for the Secure Debug verifying key provisioned to the Secure Engine.
Vendor Key ID for AES-128 key provisioned to the Secure Engine.
Vendor Key ID for the TrustZone root key.
Algorithm with which the SL_SE_BUILTIN_KEY_AES128_ID key will be used.
Macro Definition Documentation#
SL_SE_BUILTIN_KEY_APPLICATION_ATTESTATION_ID#
#define SL_SE_BUILTIN_KEY_APPLICATION_ATTESTATION_IDValue:
(MBEDTLS_PSA_KEY_ID_BUILTIN_MIN + 5)
Vendor Key ID for the built-in application identity key on Vault High devices.
99
of file platform/security/sl_component/sl_mbedtls_support/inc/sl_psa_values.h
SL_SE_BUILTIN_KEY_SYSTEM_ATTESTATION_ID#
#define SL_SE_BUILTIN_KEY_SYSTEM_ATTESTATION_IDValue:
(MBEDTLS_PSA_KEY_ID_BUILTIN_MIN + 4)
Vendor Key ID for the built-in SE identity key on Vault High devices.
104
of file platform/security/sl_component/sl_mbedtls_support/inc/sl_psa_values.h
SL_SE_BUILTIN_KEY_SECUREBOOT_ID#
#define SL_SE_BUILTIN_KEY_SECUREBOOT_IDValue:
(MBEDTLS_PSA_KEY_ID_BUILTIN_MIN + 1)
Vendor Key ID for the Secure Boot verifying key provisioned to the Secure Engine.
110
of file platform/security/sl_component/sl_mbedtls_support/inc/sl_psa_values.h
SL_SE_BUILTIN_KEY_SECUREDEBUG_ID#
#define SL_SE_BUILTIN_KEY_SECUREDEBUG_IDValue:
(MBEDTLS_PSA_KEY_ID_BUILTIN_MIN + 2)
Vendor Key ID for the Secure Debug verifying key provisioned to the Secure Engine.
115
of file platform/security/sl_component/sl_mbedtls_support/inc/sl_psa_values.h
SL_SE_BUILTIN_KEY_AES128_ID#
#define SL_SE_BUILTIN_KEY_AES128_IDValue:
(MBEDTLS_PSA_KEY_ID_BUILTIN_MIN + 3)
Vendor Key ID for AES-128 key provisioned to the Secure Engine.
120
of file platform/security/sl_component/sl_mbedtls_support/inc/sl_psa_values.h
SL_SE_BUILTIN_KEY_TRUSTZONE_ID#
#define SL_SE_BUILTIN_KEY_TRUSTZONE_IDValue:
(MBEDTLS_PSA_KEY_ID_BUILTIN_MIN + 6)
Vendor Key ID for the TrustZone root key.
125
of file platform/security/sl_component/sl_mbedtls_support/inc/sl_psa_values.h
SL_SE_BUILTIN_KEY_AES128_ALG#
#define SL_SE_BUILTIN_KEY_AES128_ALGValue:
(SL_SE_BUILTIN_KEY_AES128_ALG_CONFIG)
Algorithm with which the SL_SE_BUILTIN_KEY_AES128_ID key will be used.
131
of file platform/security/sl_component/sl_mbedtls_support/inc/sl_psa_values.h