Battery Monitor Callbacks#
These callbacks are contributed by the Battery Monitor plugin.
Functions#
void
emberAfPluginBatteryMonitorDataReadyCallback(uint16_t batteryVoltageMilliV)
Data Ready.
Function Documentation#
emberAfPluginBatteryMonitorDataReadyCallback#
void emberAfPluginBatteryMonitorDataReadyCallback (uint16_t batteryVoltageMilliV)
Data Ready.
Parameters
N/A | batteryVoltageMilliV | The battery voltage, in milli Volts Ver.: always |
This function is called whenever the battery monitor has generated a new valid battery level.
Definition at line
97
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/ncp/doc/callback.doc