Radio Coexistence Callbacks#
These callbacks are contributed by the Radio Coexistence plugin.
Functions#
void
coexCoulombCounterEventCallback(uint16_t ccState)
Reports a change in radio state.
Function Documentation#
coexCoulombCounterEventCallback#
void coexCoulombCounterEventCallback (uint16_t ccState)
Reports a change in radio state.
Parameters
N/A | ccState | bitmask of radio states |
This function is called by the RAIL library to report changes in the radio states (Idle/Rx/Tx) according to PTA events.
Definition at line
368
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/ncp/doc/callback.doc