Microphone IMAADPCM Callbacks#
These callbacks are contributed by the Microphone IMAADPCM plugin.
Functions#
void
halMicrophoneImaadpcmDataReadyCallback(uint8_t *data, uint8_t length)
Called when new microphone data is ready.
Function Documentation#
halMicrophoneImaadpcmDataReadyCallback#
void halMicrophoneImaadpcmDataReadyCallback (uint8_t * data, uint8_t length)
Called when new microphone data is ready.
Parameters
N/A | data | Pointer to the data that is ready. |
N/A | length | Length of the data. |
@appusage This function is called by the plugin when new data has been processed and is ready to be processed by other parts of the system.
Definition at line
692
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/ncp/doc/callback.doc