HAL Library Callbacks#
These callbacks are contributed by the HAL Library plugin.
Functions#
void
halRadioPowerUpHandler(void)
Called whenever the radio is powered on.
void
halRadioPowerDownHandler(void)
Called whenever the radio is powered off.
void
halSleepCallback(boolean enter, SleepModes sleepMode)
Called whenever the microcontroller enters/exits a idle/sleep mode.
Function Documentation#
halRadioPowerUpHandler#
void halRadioPowerUpHandler (void )
Called whenever the radio is powered on.
Parameters
N/A |
Definition at line
544
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/ncp/doc/callback.doc
halRadioPowerDownHandler#
void halRadioPowerDownHandler (void )
Called whenever the radio is powered off.
Parameters
N/A |
Definition at line
551
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/ncp/doc/callback.doc
halSleepCallback#
void halSleepCallback (boolean enter, SleepModes sleepMode)
Called whenever the microcontroller enters/exits a idle/sleep mode.
Parameters
N/A | enter | True if entering idle/sleep, False if exiting |
N/A | sleepMode | Idle/sleep mode |
Definition at line
561
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/ncp/doc/callback.doc