Tamper Switch Interface Callbacks#

These callbacks are contributed by the Tamper Switch Interface plugin.

Functions#

Function Documentation#

emberAfPluginTamperSwitchTamperActiveCallback#

void emberAfPluginTamperSwitchTamperActiveCallback (void )

Tamper is active.

Parameters
N/A

This function is called whenever the tamper switch detects that it has entered the enclosure, thereby activating tamper monitoring.


Definition at line 923 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/ncp/doc/callback.doc

emberAfPluginTamperSwitchTamperAlarmCallback#

void emberAfPluginTamperSwitchTamperAlarmCallback (void )

Tamper alarm.

Parameters
N/A

This function is called when the plugin detects that the enclosure has been opened.


Definition at line 933 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/ncp/doc/callback.doc