Application information. During the commissioning of GPD that supports generic switch, multi sensor extension and compact report attribute the application information is exchanged as part of the GPD commissioning command 0xE0 and 0xE4. This structure holds the information for the commissioned GPD.
Public Attributes#
Public Attribute Documentation#
deviceId#
uint8_t EmberGpApplicationInfo::deviceId
Device ID of the GPD
495
of file stack/include/gp-types.h
applInfoBitmap#
uint8_t EmberGpApplicationInfo::applInfoBitmap
Application Information bitmap
497
of file stack/include/gp-types.h
manufacturerId#
uint16_t EmberGpApplicationInfo::manufacturerId
Manufacturer ID of the GPD
499
of file stack/include/gp-types.h
modelId#
uint16_t EmberGpApplicationInfo::modelId
Model ID of the GPD
501
of file stack/include/gp-types.h
numberOfGpdCommands#
uint8_t EmberGpApplicationInfo::numberOfGpdCommands
Number of GPD commands supported by the GPD
503
of file stack/include/gp-types.h
gpdCommands#
uint8_t EmberGpApplicationInfo::gpdCommands[GP_COMMISSIONING_MAX_BYTES - 1]
Supported GPD Commands
505
of file stack/include/gp-types.h
numberOfPairedEndpoints#
uint8_t EmberGpApplicationInfo::numberOfPairedEndpoints
Number of paired endpoints for the GPD
507
of file stack/include/gp-types.h
pairedEndpoints#
uint8_t EmberGpApplicationInfo::pairedEndpoints[GP_COMMISSIONING_MAX_BYTES - 1]
Paired endpoints
509
of file stack/include/gp-types.h
numberOfGpdClientCluster#
uint8_t EmberGpApplicationInfo::numberOfGpdClientCluster
Number of operational client clusters present on the GPD, maximum is 15.
511
of file stack/include/gp-types.h
numberOfGpdServerCluster#
uint8_t EmberGpApplicationInfo::numberOfGpdServerCluster
Number of operational server clusters present on the GPD, maximum is 15.
513
of file stack/include/gp-types.h
serverClusters#
uint16_t EmberGpApplicationInfo::serverClusters[15]
Operational server clusters present on the GPD
515
of file stack/include/gp-types.h
clientClusters#
uint16_t EmberGpApplicationInfo::clientClusters[15]
Operational client clusters present on the GPD
517
of file stack/include/gp-types.h