GP Tx queue entry.
Public Attribute Documentation#
inUse#
bool EmberGpTxQueueEntry::inUse
The entry in use
Definition at line
419
of file stack/include/gp-types.h
useCca#
bool EmberGpTxQueueEntry::useCca
Use CCA during transmit
Definition at line
421
of file stack/include/gp-types.h
addr#
EmberGpAddress EmberGpTxQueueEntry::addr
GP address
Definition at line
423
of file stack/include/gp-types.h
gpdCommandId#
uint8_t EmberGpTxQueueEntry::gpdCommandId
GPD Command ID
Definition at line
425
of file stack/include/gp-types.h
asdu#
EmberMessageBuffer EmberGpTxQueueEntry::asdu
Buffer holding ASDU
Definition at line
427
of file stack/include/gp-types.h
gpepHandle#
uint8_t EmberGpTxQueueEntry::gpepHandle
Handle for the outgoing message
Definition at line
429
of file stack/include/gp-types.h
queueEntryLifetimeMs#
uint16_t EmberGpTxQueueEntry::queueEntryLifetimeMs
Life time in milliseconds for the entry to expire, 0 indicates no expiry
Definition at line
431
of file stack/include/gp-types.h