Generic Switch Information. Generic switch feature uses this as descriptor to interpret the incoming switch command from the GPD. This information is set up at the sink during the commissioning.
Public Attribute Documentation#
switchInfoLength#
uint8_t EmberGpSwitchInformation::switchInfoLength
Switch Information Length
Definition at line
597
of file stack/include/gp-types.h
nbOfContacts#
uint8_t EmberGpSwitchInformation::nbOfContacts
Number of contacts in the switch
Definition at line
599
of file stack/include/gp-types.h
switchType#
uint8_t EmberGpSwitchInformation::switchType
Switch type
Definition at line
601
of file stack/include/gp-types.h
currentContact#
uint8_t EmberGpSwitchInformation::currentContact
Current contact
Definition at line
603
of file stack/include/gp-types.h
savedContact#
uint8_t EmberGpSwitchInformation::savedContact
Saved contacts
Definition at line
605
of file stack/include/gp-types.h