The internal representation of a proxy table entry.

Public Attribute Documentation#

status#

EmberGpProxyTableEntryStatus EmberGpProxyTableEntry::status

Internal status. Defines if the entry is unused or used as a proxy entry


Definition at line 237 of file stack/include/gp-types.h

options#

uint32_t EmberGpProxyTableEntry::options

The tunneling options (this contains both options and extendedOptions from the spec)


Definition at line 241 of file stack/include/gp-types.h

gpd#

EmberGpAddress EmberGpProxyTableEntry::gpd

The addressing info of the GPD


Definition at line 245 of file stack/include/gp-types.h

assignedAlias#

EmberNodeId EmberGpProxyTableEntry::assignedAlias

The assigned alias for the GPD


Definition at line 249 of file stack/include/gp-types.h

securityOptions#

uint8_t EmberGpProxyTableEntry::securityOptions

The security options field


Definition at line 253 of file stack/include/gp-types.h

gpdSecurityFrameCounter#

EmberGpSecurityFrameCounter EmberGpProxyTableEntry::gpdSecurityFrameCounter

The SFC of the GPD


Definition at line 257 of file stack/include/gp-types.h

gpdKey#

EmberKeyData EmberGpProxyTableEntry::gpdKey

The key for the GPD.


Definition at line 261 of file stack/include/gp-types.h

sinkList#

EmberGpSinkListEntry EmberGpProxyTableEntry::sinkList[GP_SINK_LIST_ENTRIES]

The list of sinks; hardcoded to 2, which is the spec minimum


Definition at line 265 of file stack/include/gp-types.h

groupcastRadius#

uint8_t EmberGpProxyTableEntry::groupcastRadius

The groupcast radius


Definition at line 269 of file stack/include/gp-types.h

searchCounter#

uint8_t EmberGpProxyTableEntry::searchCounter

The search counter


Definition at line 273 of file stack/include/gp-types.h