Configuration of CC Association Group Information#
Modules#
Functions#
const cc_agi_config_t *
cc_agi_get_config(void)
Returns the address of the first element in the configuration array.
uint8_t
cc_agi_config_get_group_count_by_endpoint(uint8_t endpoint)
Returns the number of configured groups for a given endpoint.
const cc_agi_group_t *
Returns the address of the first element in the array of root device groups.
Function Documentation#
cc_agi_get_config#
const cc_agi_config_t * cc_agi_get_config (void )
Returns the address of the first element in the configuration array.
Parameters
N/A |
Returns
Address of the first element in the CC AGI configuration.
Definition at line
44
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Association/inc/cc_agi_config_api.h
cc_agi_config_get_group_count_by_endpoint#
uint8_t cc_agi_config_get_group_count_by_endpoint (uint8_t endpoint)
Returns the number of configured groups for a given endpoint.
Parameters
N/A | endpoint | Endpoint. |
Returns
Number of groups.
Definition at line
51
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Association/inc/cc_agi_config_api.h
cc_agi_get_rootdevice_groups#
const cc_agi_group_t * cc_agi_get_rootdevice_groups (void )
Returns the address of the first element in the array of root device groups.
Parameters
N/A |
Note
The first element is group 2.
Returns
Address of first element in root device group array.
Definition at line
60
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Association/inc/cc_agi_config_api.h