Defines the different types that a value can take, e.g.
uint8_t, int16_t, etc.
Public Attribute Documentation#
as_uint32#
uint32_t cc_config_parameter_value_t::as_uint32
Definition at line
66
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
as_uint16#
uint16_t cc_config_parameter_value_t::as_uint16
Definition at line
67
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
as_uint8#
uint8_t cc_config_parameter_value_t::as_uint8
Definition at line
68
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
as_int32#
int32_t cc_config_parameter_value_t::as_int32
Definition at line
70
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
as_int16#
int16_t cc_config_parameter_value_t::as_int16
Definition at line
71
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
as_int8#
int8_t cc_config_parameter_value_t::as_int8
Definition at line
72
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h
as_uint8_array#
uint8_t cc_config_parameter_value_t::as_uint8_array[4]
Definition at line
74
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Configuration/inc/CC_Configuration.h