Public Attributes#
const uint8_t
const notification_type_t
const agi_profile_t
const notification_event_state *
const uint8_t
Current event state.
Public Attribute Documentation#
rxOpt#
RECEIVE_OPTIONS_TYPE_EX _cc_notification_t::rxOpt
Definition at line
35
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h
endpoint#
const uint8_t _cc_notification_t::endpoint
Definition at line
36
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h
type#
const notification_type_t _cc_notification_t::type
Definition at line
37
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h
agi_profile#
const agi_profile_t _cc_notification_t::agi_profile
Definition at line
38
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h
events#
const notification_event_state* _cc_notification_t::events
Definition at line
39
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h
event_count#
const uint8_t _cc_notification_t::event_count
Definition at line
40
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h
current_event#
notification_event_state _cc_notification_t::current_event
Definition at line
41
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h
status#
NOTIFICATION_STATUS _cc_notification_t::status
Current event state.
Definition at line
42
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/src/cc_notification_config_api.h