Structure used by supervision_event_handler() to process upcoming events Registered for CC Supervision.
Public Attributes#
zaf_tx_options_t
uint8_t
TX data to be used to send Supervision Report.
bool
Supervision session Id.
uint8_t
Status Update. True if more reports will follow.
Public Attribute Documentation#
tx_options#
zaf_tx_options_t _cc_supervision_report_event::tx_options
Definition at line
118
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
session_id#
uint8_t _cc_supervision_report_event::session_id
TX data to be used to send Supervision Report.
Definition at line
119
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
status_update#
bool _cc_supervision_report_event::status_update
Supervision session Id.
Definition at line
120
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h
duration#
uint8_t _cc_supervision_report_event::duration
Status Update. True if more reports will follow.
Definition at line
121
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h