This struct is used for the arguments in cc_supervision_get_receive_handler function pointer in init_and_reset.

Public Attributes#

uint8_t

Input.

uint8_t

Input.

uint8_t

Input: bit[0..5] session id, bit[7] status update disable/enable.

uint8_t

Output.

Public Attribute Documentation#

cmdClass#

uint8_t SUPERVISION_GET_RECEIVED_HANDLER_ARGS::cmdClass

Input.


Definition at line 103 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h

cmd#

uint8_t SUPERVISION_GET_RECEIVED_HANDLER_ARGS::cmd

Input.


Definition at line 104 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h

properties1#

uint8_t SUPERVISION_GET_RECEIVED_HANDLER_ARGS::properties1

Input: bit[0..5] session id, bit[7] status update disable/enable.

Output: bit[0..5] session id, bit[7] more status updates of type cc_supervision_more_status_updates_t


Definition at line 105 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h

status#

cc_supervision_status_t SUPERVISION_GET_RECEIVED_HANDLER_ARGS::status

Output.


Definition at line 107 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h

duration#

uint8_t SUPERVISION_GET_RECEIVED_HANDLER_ARGS::duration

Output.


Definition at line 108 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h

rxOpt#

RECEIVE_OPTIONS_TYPE_EX* SUPERVISION_GET_RECEIVED_HANDLER_ARGS::rxOpt

Input.


Definition at line 109 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Supervision/inc/CC_Supervision.h