Public Attributes#
uint8_t
The raw buffer which holds the result.
The precision which the raw result should be interpret with.
The size which the raw result should be interpret with.
Public Attribute Documentation#
raw_result#
uint8_t _sensor_read_result::raw_result[SLI_MAX_RAW_RESULT_BYTES]
The raw buffer which holds the result.
Definition at line
98
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h
precision#
sensor_read_result_precision _sensor_read_result::precision
The precision which the raw result should be interpret with.
Definition at line
99
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h
size_bytes#
sensor_read_result_size_t _sensor_read_result::size_bytes
The size which the raw result should be interpret with.
Definition at line
100
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h