Structure that holds the attributes of a sensor type.

Public Attributes#

uint8_t

Sensor type id from SDS13812.

uint8_t

Supported bitmask byte number from SDS13812.

uint8_t

Supported bitmask bit number from SDS13812.

uint8_t

Maximum supported scale number from SDS13812.

Public Attribute Documentation#

value#

uint8_t _sensor_type::value

Sensor type id from SDS13812.


Definition at line 67 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

byte_offset#

uint8_t _sensor_type::byte_offset

Supported bitmask byte number from SDS13812.


Definition at line 68 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

bit_mask#

uint8_t _sensor_type::bit_mask

Supported bitmask bit number from SDS13812.


Definition at line 69 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

max_scale_value#

uint8_t _sensor_type::max_scale_value

Maximum supported scale number from SDS13812.


Definition at line 70 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h