Z-Wave Radio Configuration#
Z-Wave Radio Configuration.
Macro Definition Documentation#
ZW_REGION#
#define ZW_REGIONValue:
REGION_DEFAULT
The supported region of the device.
Used only if region value is not previously written in MFG_ZWAVE_COUNTRY_FREQ token. To delete value from MFG token, run: commander flash –tokengroup znet –token MFG_ZWAVE_COUNTRY_FREQ:0xFF
The supported region of the device. Used only if region value is not previously written in MFG_ZWAVE_COUNTRY_FREQ token. To delete value from MFG token, run: commander flash –tokengroup znet –token MFG_ZWAVE_COUNTRY_FREQ:0xFF
Option | Value |
---|---|
Default (Europe) | REGION_DEFAULT |
Australia / New Zealand | REGION_ANZ |
China | REGION_CN |
Europe | REGION_EU |
Hong Kong | REGION_HK |
Israel | REGION_IL |
India | REGION_IN |
Japan | REGION_JP |
Korea | REGION_KR |
Russia | REGION_RU |
United States | REGION_US |
United States Long Range | REGION_US_LR |
46
of file /mnt/raid/workspaces/ws.5ZeoF8fvV/overlay/gsdk/protocol/z-wave/config/zw_region_config.h