Public Attributes#

ZW_APPLICATION_TX_BUFFER *
uint8_t

Public Attribute Documentation#

rx_options#

RECEIVE_OPTIONS_TYPE_EX* _cc_handler_input_t::rx_options

Definition at line 198 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

frame#

ZW_APPLICATION_TX_BUFFER* _cc_handler_input_t::frame

Definition at line 199 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

length#

uint8_t _cc_handler_input_t::length

Definition at line 200 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h