Defines the first two elements for all CC configurations.

Public Attribute Documentation#

rxOpt#

RECEIVE_OPTIONS_TYPE_EX zaf_cc_config_t::rxOpt

Definition at line 475 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

endpoint#

uint8_t zaf_cc_config_t::endpoint

Definition at line 476 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h