Properties of the received frame.

Used mostly by command classes to prepare response to a command.

Public Attributes#

uint8_t

Frame header info.

uint8_t

true if supervision is active

uint8_t

Current sessionId.

uint8_t

Is statusUpdate enabled for current session.

Public Attribute Documentation#

rxStatus#

uint8_t _RECEIVE_OPTIONS_TYPE_EX_::rxStatus

Frame header info.


Definition at line 68 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

securityKey#

security_key_t _RECEIVE_OPTIONS_TYPE_EX_::securityKey

Definition at line 69 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

sourceNode#

MULTICHAN_SOURCE_NODE_ID _RECEIVE_OPTIONS_TYPE_EX_::sourceNode

Definition at line 70 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

destNode#

MULTICHAN_DEST_NODE_ID _RECEIVE_OPTIONS_TYPE_EX_::destNode

Definition at line 71 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

bSupervisionActive#

uint8_t _RECEIVE_OPTIONS_TYPE_EX_::bSupervisionActive

true if supervision is active


Definition at line 72 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

sessionId#

uint8_t _RECEIVE_OPTIONS_TYPE_EX_::sessionId

Current sessionId.


Definition at line 73 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

statusUpdate#

uint8_t _RECEIVE_OPTIONS_TYPE_EX_::statusUpdate

Is statusUpdate enabled for current session.


Definition at line 74 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h