First generation of the CC handler item.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

CC#

uint16_t CC_handler_map_t::CC

Definition at line 247 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

version#

uint16_t CC_handler_map_t::version

Definition at line 248 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

pHandler#

cc_handler_t CC_handler_map_t::pHandler

Definition at line 249 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h