Public Attributes#

void(*
uint8_t

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.

uint8_t

Public Attribute Documentation#

pHandle#

void(* SCommandNetworkManagementDSK::pHandle) (void)

Definition at line 1767 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

mode#

uint8_t SCommandNetworkManagementDSK::mode

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.


Definition at line 1770 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

dsk#

uint8_t SCommandNetworkManagementDSK::dsk[8]

Definition at line 1771 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h