Public Attributes#

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

nodeID#

uint8_t SCommandSetRoutingInfo::nodeID

Definition at line 1458 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

length#

uint8_t SCommandSetRoutingInfo::length

Definition at line 1459 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

nodeMask#

uint8_t SCommandSetRoutingInfo::nodeMask[MAX_NODEMASK_LENGTH]

Definition at line 1460 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h