Public Attribute Documentation#

Payload#

UReceiveCmdPayload SReceiveSingle::Payload

Definition at line 2158 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

iLength#

uint8_t SReceiveSingle::iLength

Definition at line 2159 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

RxOptions#

RECEIVE_OPTIONS_TYPE SReceiveSingle::RxOptions

Definition at line 2160 of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h