Public Attributes#
void(*
Will be returned with transmit status Allows application to recognize frames.
uint8_t
uint8_t
uint8_t
Public Attribute Documentation#
Handle#
void(* STransmitFrameConfig::Handle) (uint8_t txStatus, TX_STATUS_TYPE *extendedTxStatus)
Will be returned with transmit status Allows application to recognize frames.
Definition at line
1648
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
TransmitOptions#
uint8_t STransmitFrameConfig::TransmitOptions
Definition at line
1649
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
iFrameLength#
uint8_t STransmitFrameConfig::iFrameLength
Definition at line
1650
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
aFrame#
uint8_t STransmitFrameConfig::aFrame[TX_BUFFER_SIZE]
Definition at line
1651
of file /mnt/raid/workspaces/ws.WH1KakGoP/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h