Stream Settings

stream.auto_close

Abbreviation

st a

Access

get/set

Description

This setting is intended for all network related streams:

When stream.auto_close is false , a stream remains open until the stream_close command is sent. Use the stream_poll command to determine status. A stream status of 2 indicates that the stream connection has been closed remotely. In this case, read any remaining RX data in the stream and issue stream_close .

When stream.auto_close is true , a stream handle is automatically reused when closed remotely.

Note: When stream.auto_close is true , TCP/HTTP/WebSocket client/server streams remain open until all RX data has been read, even if the remote side has closed the connection.

Arguments

<1|true|on/0|false|off>

where

Default

0

Properties

Get example

> get st a
0
>

Set example

> set st a true
Set OK