System

system.build_number

Abbreviation

sy n (in some versions: sy b n )

Access

get

Description

Returns Gecko OS build number.

Arguments

None

Default

N/A

Platforms

Get example

> get sy n
R000009
16eee81

system.cmd.buffered

Abbreviation

sy c b

Access

get/set

Description

Flag to enable/disable buffering of certain command responses. This is intended for use when reading command output by machine. See Serial Interface, Command Protocol .

If enabled, a command's response is buffered and a stream handle along with the response size in bytes is returned.

The host must use the read command to retrieve the command's response data.

Note that if headers are enabled, the header is returned along with the stream handle and response size.

The following commands are buffered if the system.cmd.buffered flag is set:

Stream Type : CMD . See Networking and Security, Network Connections and Streams .

Arguments

0|off|false/1|on|true

Default

0

Properties

Platforms

Get example

> get sy c b
0

Set example

> set sy c b on
Set OK

system.cmd.echo

Abbreviation

sy c e

Access

get/set

Description

Enable/disable character echo. Only applies to command mode.

Arguments

0|off|false/1|on|true>

Default

1

Properties

Platforms

Get example

> get sy c e
R000003
1

Set example

> set sy c e on
R000008
Set OK

system.cmd.format

Abbreviation

sy c f

Access

set

Description

Puts the Gecko OS command interface into human or machine format. For further details, see Serial Interface, Command Format Configuration .

Note : This variable is NOT readable.

Arguments

<human | machine>

Default

human

Properties

Set example

> set sy c f human
R000008
Set OK

system.cmd.header_enabled

Abbreviation

sy c h

Access

get/set

Description

Enable/disable a response header for commands. Only applies to command mode. Response headers make it easy to parse responses with a host MCU.

Arguments

0|off|false/1|on|true>

Default

0

Properties

Platforms

Get example

> get sy c h
R000003
1

Set example

> set sy c h on
R000008
Set OK

system.cmd.prompt_enabled

Abbreviation

sy c p

Access

get/set

Description

Enable/disable terminal command prompt. Only applies to command mode. A prompt makes it easy for humans to interact with Gecko OS.

Arguments

0|off|false/1|on|true>

Default

1

Properties

Platforms

Get example

> get sy c p
R000003
1

Set example

> set sy c p on
R000008
Set OK

system.gotosleep.timeout

Abbreviation

sy s t

Access

get/set

Description

The module automatically goes to sleep after a timeout period of <seconds> . The timeout countdown restarts when a wake event occurs and is held off if data is available on open network connections, the minimum timeout is 10 seconds. 0 disables gotosleep. A save and reboot is required before the sleep timeout is enabled.

Arguments

<seconds>

Default

0

Properties

Platforms

Get example

> get sy s t
R000003
0

Set example

> set sy s t 12
R000008
Set OK

system.indicator.gpio

Abbreviation

sy i g

Access

get/set

Description

The GPIO used for a particular system indicator. System indicators drive LEDs to indicate the state of the wlan, network and softap interfaces. -1 to disable.

Arguments

<wlan/network/softap> <GPIO#>

Default

<varies>

Properties

Platforms

Get example

> get sy i g network
R000004
11

Set example

> set gpio.alias 11 netstat_gpio   <- Alias GPIO 11 for simplicity
R000008
Set OK
> set sy i g network netstat_gpio
R000008
Set OK

system.indicator.state

Abbreviation

sy i s

Access

get/set

Description

System indicator option for each state as described in the following tables.

WLAN Indicator

Wi-Fi Client status, by default unassigned on eval boards

State # State Description Default Behavior
state 1 Wi-Fi off static_off
state 2 Error fast_blink
state 3 Connecting to AP medium_blink
state 4 Joined to AP slow_blink

Network Indicator

Network status, by default GREEN LED on eval boards

State # State Description Default Behavior
state 1 No IP address fast_blink
state 2 DHCP in-progress medium_blink
state 3 DHCP successful slow_blink

SoftAP Indicator

SoftAP status, by default RED LED on eval boards

State # State Description Default Behavior
state 1 SoftAP off static_off
state 2 SoftAP error fast_blink
state 3 SoftAP active medium_blink
state 4 Client connected slow_blink

Arguments

<wlan/network/softap> <csv list>

Default

See above:

Properties

Platforms

Get example

> get sy i s wlan
R000047
static_off|fast_blink|medium_blink|slow_blink

Set example

> set sy i s network static_off|medium_blink|static_on
R000008
Set OK

system.memory.usage

Abbreviation

sy e u

Access

get

Description

Returns the heap memory currently in use, as a percentage of total heap memory. See Memory .

Arguments

-

Default

-

Platforms

Get example

> get sy e u
58

system.oob.event_mask

Abbreviation

sy o e

Access

get/set

Description

The mask of events which assert the OOB GPIO.

For event/mask mapping, see the system.oob.gpio event mask table .

Arguments

<hex mask> Mask is specified in the form 0xHH where H is a hexadecimal digit 0-F.

Default

0x0

Properties

Platforms

Get example

> get sy o e
0x1F

Set example

> set sy o e 0x11
Set OK

system.oob.gpio

Abbreviation

sy o g

Access

get/set

Description

The system.oob variables allow creation of an out-of-band interrupt (OOB) GPIO. This GPIO is asserted whenever one or more of the configured OOB events occurs. It is de-asserted when reading the OOB status register.

Note : OOB events are in most cases related to a corresponding special function GPIO variable. However, the OOB event can be configured without setting the corresponding special function GPIO.

Specify the OOB GPIO with the system.oob.gpio variable.

Specify the active level of the OOB GPIO with system.oob.gpio_level .

Specify the events that cause the OOB GPIO to be asserted with system.oob.event_mask .

Specify events that trigger the OOB GPIO only on the rising edge (i.e. when the event is asserted) with system.oob.rising_edge_mask .

Read the events that triggered an OOB interrupt from the system.oob.status variable.

Only one GPIO can be specified as the OOB GPIO. Determine the OOB GPIO by reading the gpio.usage variable or the system.oob.gpio variable.

Events are mapped to the event mask , rising edge mask and status mask as shown in the following table:

OOB Event Name Mask Value
ioconn.status_gpio 0x001
tcp.server.connected_gpio 0x004
tcp.server.data_gpio 0x008
HTTP data ready (see http_get , http_post commands) 0x400

Arguments

<GPIO #> The number of the OOB GPIO.

Default

No GPIO assigned to OOB

Properties

Platforms

Get example

> get sy o g
22

Set example

> set system.oob.gpio 22
Set OK

system.oob.gpio_level

Abbreviation

sy o l

Access

get/set

Description

The active level of the OOB GPIO. See system.oob.gpio .

Arguments

<0/1>

Default

1

Properties

Platforms

Get example

> get sy o l
1

Set example

> set sy o l 0
Set OK

system.oob.rising_edge_mask

Abbreviation

sy o r

Access

get/set

Description

The mask of events which should trigger the OOB GPIO only on the rising edge (i.e. when an event is asserted). See system.oob.gpio .

If the mask is cleared, then the OOB GPIO is asserted on both rising and falling edges.

For instance, when the module connects, the network status event event is considered asserted. When the module disconnects, the event is considered de-asserted.

For event/mask mapping, see the system.oob.gpio event mask table .

Arguments

<hex mask> Mask is specified in the form 0xHH where H is a hexadecimal digit 0-F.

Default

0x0

Properties

Platforms

Get example

> get sy o r
0x1F

Set example

> set sy o r 0x11
Set OK

system.oob.status

Abbreviation

sy o s

Access

get

Description

The mask of triggered events. When an event is triggered, the OOB GPIO is asserted and the status mask is updated with the triggering event. Reading this variable returns a mask of events that caused the OOB gpio to be asserted.

Reading this variable de-asserts the OOB GPIO and clears the status mask.

For event/mask mapping, see the system.oob.gpio event mask table .

Arguments

-

Default

0x0

Platforms

Get example

get sy o e
0x0

system.print_level

Abbreviation

sy p

Access

get/set

Description

Print levels:

Each print level includes lower levels.

Set system.print_level to 0 to disable all system and log messages.

Arguments

<[0-4]/[all]>

Default

all

Properties

Platforms

Get example

> get sy p
R000005
all

Set example

> set sy p 0
R000008
Set OK

system.safemode.status

Abbreviation

sy s

Access

get

Description

Returns a flag to indicate whether the system is in safe mode. The module switches to safe mode after eight exceptions occur with the boot application.

Arguments

-

Default

0

Properties

Platforms

Get example

> get sy s
R000003
0

system.safemode.disabled

Abbreviation

sy d

Access

get/set

Description

Disables safe mode feature when set to true . When safe mode is disabled and 8 or more faults occur, Gecko OS automatically resets the fault counter and runs the boot application. It is strongly recommended to leave this setting false as it may not be possible to recover from a fatal error.

Note : A factory reset returns this setting to the default state of false .

Arguments

<true/1/0/false>

Default

0

Properties

Platforms

Get example

> get sy d
R000003
0

Set example

> set sy d 1
R000009
Success

system.uuid

Abbreviation

sy u

Access

get

Description

Returns the hardware UUID of the module.

Arguments

Default

Properties

Platforms

Get example

> get sy u
R000042
05B3203FA03133434E39423330363031B2303533

system.version

Abbreviation

sy v

Access

get

Description

Returns the Gecko OS firmware bundle version.

Arguments

-

Default

<varies>

Properties

Platforms

Get example

> get sy v
R000052
SILABS-AMW007-2.1.5, Gecko OS-2.1.5, AMW007-W00001

system.wakeup.timeout

Abbreviation

sy w t

Access

get/set

Description

The module automatically wakes from sleep after timeout . 0 disables auto-wakeup.

Arguments

<seconds>

Default

0

Properties

Platforms

Get example

> get sy w t
R000003
0

Set example

> set sy w t 60
R000008
Set OK