TCP Client

tcp.client.auto_interface

Abbreviation

tc c i

Access

get/set

Description

Interface to auto-start TCP client connection.

See TCP Client .

Arguments

default

Default

<default/wlan/softap>

Properties

Get example

> get tcp.client.auto_interface
default

Set example

> set tc c i wlan
Set OK

tcp.client.auto_retries

Abbreviation

tc c e

Access

get/set

Description

Determines number of attempts to reconnect after remote server disconnects client.

To control how the client connects to the server, use tcp.client.retries , tcp.client.connect_timeout and tcp.client.retry_period .

See TCP Client .

Arguments

<0-255>

Default

0

Properties

Platforms

Get example

> get tcp.client.auto_retries
0

Set example

set tc c e 20
Set OK

tcp.client.auto_start

Abbreviation

tc c a

Access

get/set

Description

Enable/disable TCP client auto-start feature. If enabled, TCP client automatically connects to the specified tcp.client.remote_host when the network interface is brought up.

To enable TLS, see tcp.client.tls_enabled .

See TCP Client .

Note : If tcp.client.auto_start is enabled, and you close the tcp.client (TCPC) stream after it connects, you cannot open it again using the tcp_client command. To trigger tcp.client.auto_start again, restart the device network: network_restart . The TCP client then automatically reconnects.

Arguments

<0/1>

Default

0

Properties

Platforms

Get example

> get tcp.client.auto_start
0

Set example

> set tc c a 1
Set OK

tcp.client.connect_timeout

Abbreviation

tc c t

Access

get/set

Description

TCP client connect timeout in milliseconds.

This variable controls timeout for the following commands:

See TCP Client .

Arguments

<milliseconds>

Default

5000

Properties

Platforms

Get example

> get tc c t
R000006
5000

Set example

> set tc c t 6500
R000008
Set OK

tcp.client.connected_str

Abbreviation

tc c c

Access

get/set

Description

Set the value of a message displayed on the Gecko OS terminal (sent to the UART), when the device auto connects as a TCP client to a TCP server, in stream mode.

Note : This message is displayed only when the device is in STREAM mode .

See TCP Client .

Arguments

<message>

Default

Empty string

Platforms

Set example

> set tc c c *READY*
R000008
Set OK

Get example

> get tc c c
R000009
*READY*

tcp.client.disconnected_str

Abbreviation

tc c d

Access

get/set

Description

Set the value of a message displayed on the Gecko OS terminal (sent to the UART), when the device disconnects as a TCP client from a TCP server, in stream mode.

Note : This message is displayed only when the device is in STREAM mode .

See TCP Client .

Arguments

<message>

Default

Empty string

Platforms

Set example

> set tc c d *CLOSED*
R000008
Set OK

Get example

> get tc c d
R000010
*CLOSED*

tcp.client.local_port

Abbreviation

tc c p

Access

get/set

Description

TCP client local port. 0 = automatic.

If you set this value, the first connection is made using the specified local port.

Subsequent additional TCP client connections determine the port by incrementing the last port used. If the specified port is X, the first subsequent connection uses port X+1. The next TCP client connection uses port X+2, and so on.

To reset the local port back to X, reboot the client.

See TCP Client .

Arguments

<port>

Default

0

Properties

Platforms

Get example

> get tc c p
R000003
0

Set example

> set tc c p 30009
R000008
Set OK

tcp.client.remote_host

Abbreviation

tc c h

Access

get/set

Description

Domain or IP address of remote tcp server to auto connect.

See TCP Client .

Arguments

<domain/ip address>

Default

null

Properties

Platforms

Get example

> get tcp.client.remote_host
mydomain.com

Set example

> set tc c h mydomain.com
Set OK

tcp.client.remote_port

Abbreviation

tc c o

Access

get/set

Description

Port of remote tcp server to auto connect.

See TCP Client .

Arguments

<port>

Default

3000

Properties

Platforms

Get example

> get tcp.client.remote_port

Set example

> set tc c o 5000
Set OK

Abbreviation

tc c s

Access

get/set

Description

Text string

See TCP Client .

Arguments

<message>

Default

Empty string

Set example

> set tc c s Hello
Set OK

Get example

> get tcp.client.remote_send
Hello

tcp.client.retries

Abbreviation

tc c r

Access

get/set

Description

Maximum TCP client connection retry attempts.

See TCP Client .

Arguments

<max #retries>

Default

3

Properties

Platforms

Get example

> get tc c r
R000003
3

Set example

> set tc c r 5
R000008
Set OK

tcp.client.retry_period

Abbreviation

tc c w

Access

get/set

Description

TCP client wait time between connection retry attempts.

See TCP Client .

Arguments

<milliseconds>

Default

1000

Properties

Platforms

Get example

> get tc c w
R000006
1000

Set example

> set tc c w 2000
R000008
Set OK

tcp.client.tls_enabled

Abbreviation

tc c s

Access

get/set

Description

Enables TLS for the tcp.client.auto_start feature.

The TLS certs are configured with the following variables:

See TLS Client .

Arguments

<0/1> where

Default

0

Properties

Platforms

Get example

> get tc c s
0

Set example

> set tc c s 1
Set OK