App

app.debug.auto_run

Abbreviation

ap d a

Access

get/set

Description

Enable/disable App from auto running.

This variable is not saved. When power is removed the variable is reset to its default value.

By default, an App always runs on power up.

The app.debug.auto_run variable is intended for use only in a debug session, to allow inputting commands to the Gecko OS terminal.

Arguments

1|true|on/0|false|off

where 1 : enable, 0 : disable

Default

1

Platforms

Properties

Gecko OS Plugin

Get example

> get ap d a
1

Set example

> set app.debug.auto_run 0
Set OK

app.debug.ignore_settings

Abbreviation

ap d i

Access

get/set

Description

This allows manual adjustment of variable settings while debugging a Gecko OS App that loads settings using the API gos_load_app_settings() .

When app.debug.ignore_settings is set, all calls to gos_load_app_settings() are ignored. You can then load the Gecko OS app without overwriting test variable settings.

Arguments

1|true|on/0|false|off

Default

0

Platforms

Properties

Gecko OS Plugin

Get example

> get app.debug.ignore_settings
0

Set example

> set app.debug.ignore_settings 1
Set OK

app.info

Abbreviation

ap i

Access

get

Description

Print information about the current App, including App name, size, SDK version, and running status.

Arguments

None

Platforms

Gecko OS Plugin

Get example

> get app.info
SDK version : <SDK version number>
Name        : <App name>
Size        : <Size of app, in bytes>
Running     : <1 = app running, 0 = app not running>