The HTTP RESTful API
This example uses the HTTP RESTful API to interact with the device using HTTP requests. Commands are sent to the device using HTTP REST methods such as
GET
and
POST
and a simple request syntax.
Using HTTP requests, you can send any command to the device and receive the response. The Gecko OS Web App offers a full demonstration of the HTTP RESTful API. This application note demonstrates how to use the basic requests of the RESTful API.
Other ways of managing and interacting with a Gecko OS device include:
- Gecko OS Terminal - via physical connection to USB port (see Getting Started, Opening a Gecko OS Terminal )
- Wi-Fi Remote terminal - Telnet connection via Wi-Fi (see Wi-Fi Remote Terminal application note).
- For more sophisticated scripting, the Gecko OS JavaScript API provides a JavaScript wrapper around the HTTP server REST API
This demo uses the following Gecko OS features:
- Gecko OS RESTful API - for executing Gecko OS commands directly via HTTP requests. See Networking and Security, HTTP server with RESTful API .
This example demonstrates how to:
- Setup the device to connect to your local network
- Start the Gecko OS mDNS service and HTTP web server
- Use a web browser, JavaScript or cURL to send commands to the device, and receive responses from Gecko OS
Setup
To run this example follow these steps:
Connect Your Device to the Local Network
Since you'll need to configure mDNS and the web server, the quickest way to setup the device is to use a Gecko OS terminal - see Getting Started . Once you have a terminal connected, issue the following command to configure the credentials for the local network:
> network_up -s
Enable mDNS
Enable mDNS and specify the domain the device will respond to using the following commands:
set mdns.enabled 1
set mdns.name mydevice
Enable the HTTP Server
Enable the Gecko OS HTTP server and the RESTful API using the following Gecko OS commands:
set http.server.enabled 1
set http.server.api_enabled 1
Save the settings, then restart the network:
save
network_down
network_up
The device automatically starts the mDNS discovery service and the HTTP server on boot after connecting to the network.
The response from Gecko OS is similar to the following:
> Obtaining IPv4 address via DHCP
IPv4 address: 10.5.6.59
Starting mDNS
mDNS domain: mydevice.local
HTTP and REST API server listening on port: 80
[2019-01-01 | 23:48:42: Associated]
Syntax of REST API Gecko OS Commands
The format of a REST API Gecko OS command GET request is:
GET http://mydevice.local/command/<command>
For example, to issue the
ver
command:
GET http://mydevice.local/command/ver
To issue a GET request from a browser, enter the URL
http://mydevice.local/command/ver
into the browser URL address box.
The format of a REST API Gecko OS command POST request is:
POST http://mydevice.local/command/<command>
followed immediately by a json formatted structure of the form:
{
"flags" : <flags>,
"command" : "<Gecko OS command>",
"data" : "<command data>"
}
The "data" value is required by commands that expect additional data sent immediately after the command, such as
file_create
. Some of the curl examples below demonstrate how to issue an HTTP POST request.
Sending Commands from a Web Browser
Using your favorite web browser (with a network client such as a PC, phone or tablet connected to the same local network as the device), enter the following URL to retrieve the Gecko OS version string, or click the following link if this computer is connected to the same network as the device:
http://mydevice.local/command/ver
The browser responds with the Gecko OS version embedded in a JSON object, similar to the following text.
{"id":18,"code":0,"flags":0,"response":"Gecko OS 4.0, Built:2019-01-15 ... }
Troubleshooting
If you are having problems making this work, try the following
-
omit the
.localdomain in the URL, and use http://mydevice/command/ver instead. -
replace
mydevice.localwith the IP address of the device (available by reading the Gecko OS IP address variableget wlan.network.ip). The issue may be related to the operation of mDNS which has some operating system caveats. See Networking & Security, Network Discovery
How does this work?
When the Gecko OS command is entered into the web browser address box, the browser translates the URL into an HTTP
GET
request and sends the request to the device name. The operating system in your PC (or phone / tablet) translates the device name into the device IP address and sends the request to the device. On the device, the HTTP web server receives and processes the request, and then provides a response back to the server.
A few more examples are shown below. For full documentation on the Gecko OS HTTP REST API, see Networking and Security, HTTP server with RESTful API .
Read a list of files on the device:
| URL |
http://mydevice.local/command/ls
|
|
Gecko OS
Response |
{"id":2,"code":0,"flags":0,"response":"! # Size Version Filename\r\n# 0 41741 2.1.0 command_help.csv\r\n# 1 135 2.1.0 default_setup.script\r\n# 2 1897 2.1.0 favicon.ico.gz\r\n# 3 1236 2.1.0 geotrust_ca.pem\r\n# 4 212736 2.1.0 sys/kernel.bin\r\n# 5 215204 2.1.0 sys/services.bin\r\n# 6 38004 2.1.0 gecko_os_webgui.css.gz\r\n# 7 1827 2.1.0 gecko_os_webgui.html\r\n# 8 61492 2.1.0 gecko_os_webgui.js.gz\r\n# 9 210412 5.26.230 wifi_fw.bin\r\n"} |
| URL | Thermistor GPIO | Response |
|---|---|---|
http://mydevice.local/adc 7
|
7
|
|
http://mydevice.local/adc 20
|
20
|
Typical response:
{"id":104,"code":0,"flags":0,"response":"0x835\r\n"}
Open a TCP connection to Google:
http://mydevice.local/command/tcp_client google.com 80
Response:
{"id":4,"code":0,"flags":0,"response":"0\r\n"}
Read the response to the TCP client connection above:
http://mydevice.local/log
Response:
{"logs":["HTTP and REST API server listening on port: 80","[2019-01-15 - 01:09:23: Associated]\r\n> ","Resolving host: google.com","[2019-01-15 - 01:28:53: Opening: google.com:80]","Connecting (TCP): 216.58.220.142:80","[2019-01-15 - 01:28:54: Opened: 0]"]}
Sending Commands Using JavaScript XMLHttpRequest
This demonstration uses POST requests. It is possible to send GET requests using
XMLHttpRequest
, but POST is more flexible. POST has no size restrictions, and the JSON data attribute allows additional data to be sent for Gecko OS commands such as
file_create
.
Download the demonstration HTML file js_rest_post.html .
This can be run directly as a file URL, provided you enable CORS for all domains on your device.
The following Gecko OS commands set up the device to work with the demonstration HTML page:
set wlan.ssid <YOUR_SSID>
set wlan.passkey <YOUR_PASSWORD>
set wlan.auto_join.enabled 1
set http.server.enabled 1
set mdns.name mydevice
set mdns.enabled 1
set http.server.cors_origin *
save
reboot
Run the HTML file in a browser with the JavaScript developed console displayed. This shows errors that cannot be caught and displayed with the JavaScript
try
and
catch
mechanism.
You can run any Gecko OS command from this HTML. Just edit the request fields and click the
Send POST Request
button.
The demonstration JavaScript assembles the POST JSON from the request fields and makes an
XMLHttpRequest
to send the command to the device and display the response.
View the HTML source to see the JavaScript. The core of the demonstration is the
sendPost()
function.
For higher level access to the HTTP RESTful API via JavaScript, see Gecko OS JavaScript API .
Sending Commands Using cURL
Curl , a command line URL utility, may also be used to connect to the Gecko OS webserver. Curl is typically run from a PC or Linux command line for transferring data with a URL syntax. The following examples show how to use cURL with Gecko OS.
In some of the examples below, curl commands and response are shown in separate lines for readability purposes. Curl commands should be issued on a single command line.
Tip! If you are having trouble using curl, try using the
-v
verbose flag.
Gecko OS Version
| Curl Command |
|---|
curl http://mydevice.local/command/version
|
| Gecko OS Response |
|---|
{"id":18,"code":0,"flags":0, "response":"SILABS-WGM160P-4.0.0, Gecko_OS-STANDARD-4.0.12-1198, WGM160P"}
|
Curl used with a URL only issues an HTTP GET request.
Verbose file list
This example reads a verbose list of files on the device and uses the more sophisticated POST request API . Note that the double-quotes may need to be escaped with backslash characters (as shown below) on some operating systems, such as Windows.
Curl used with the
-d
(
--data
) option issues an HTTP POST request. Note that the Content-Type header must be supplied to specify that the data posted is in json format.
| Curl Command |
|---|
curl -H "Content-Type: application/json" -d "{\"flags\":0,\"command\":\"ls -v\"}" http://mydevice.local/command
|
| Gecko OS Response |
|---|
{"id":3,"code":0,"flags":0, "response":"! # Type Flags Hnd Size Version Filename\r\n # 0 e-FB 0001 82 41741 2.1.0.0 command_help.csv\r\n # 1 e-FD 0001 53 135 2.1.0.0 default_setup.script\r\n # 2 e-FE 0001 81 1897 2.1.0.0 favicon.ico.gz\r\n # 3 e-03 0001 52 1236 2.1.0.0 geotrust_ca.pem\r\n # 4 i-00 801B 0 212736 2.1.0.0 sys/kernel.bin\r\n # 5 i-81 801B 52 215204 2.1.0.0 sys/services.bin\ r\n # 6 e-FE 0001 55 38004 2.1.0.0 gecko_os_webgui.css.gz\r\n # 7 e-FE 0001 54 1827 2.1.0.0 gecko_os_webgui.html\r\n # 8 e-FE 0001 65 61492 2.1.0.0 gecko_os_webgui.js.gz\r\n # 9 e-01 0009 0 210412 5.26.230.12 wifi_fw.bin\r\n"}
|
The value of the
response
key is the return data from the command. In this case it is the list of files. This is formatted to be read on a terminal in a monospace font, with new lines where each
\r\n
character sequence appears.
Open and Read a file
Open the
default_setup.script
file located on the Gecko OS file system:
| Curl Command |
|---|
curl -H "Content-type: application/json" -d "{\"flags\":0,\"command\":\"file_open default_setup.script\"}" http://mydevice.local/command
|
| Gecko OS Response |
|---|
{"id":14, "code":0,"flags":0, "response":"0\r\n"}
|
The value of the
response
key is the return data from the command. In this case it is the stream number for the open file stream,
0
, which is used as an argument to the
stream_read
command issued below.
Read the file using the stream_read command:
| Curl Command |
|---|
curl -H "Content-type: application/json" -d "{\"flags\":0,\"command\":\"stream_read 0 300\"}" mydevice.local/command
|
| Gecko OS Response |
|---|
{"id":15,"code":0,"flags":0, "response":"network_up,-s ,Configuration network credentials\r\nset wlan.auto_join.enabled,true,Enable network auto-join\r\nsave,-,Saving settings\r\n\r\n"}
|
Supporting Gecko OS Versions
- Gecko OS 4
Change Log
| Modified | Changes |
|---|---|
| 2019-01-01 | Created |