UDP Server
udp.server.auto_interface
Abbreviation
ud s i
Access
get/set
Description
If 'auto-start' is enabled, this is the interface used when the server is set to auto-start.
If set to default
, uses the interface specified in network.default_interface.
Arguments
wlan/softap/default
Default
default
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get ud s i
R000009
default
Set example
> set ud s i softap
R000008
Set OK
udp.server.auto_start
Abbreviation
ud s a
Access
get/set
Description
Start server on power-up
Arguments
true|on|1/false|off|0
Default
0
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get ud s a
R000003
0
Set example
> set ud s a true
R000008
Set OK
udp.server.data_gpio
Abbreviation
ud s d
Access
get/set
Description
Specify a GPIO to be asserted HIGH when client data is available to be read.
Note: Disable by setting to -1
.
See also system.oob.gpio.
Arguments
<GPIO#>
Default
-1
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get ud s d
R000004
-1
Set example
> set ud s d 3
R000008
Set OK
udp.server.lock_client
Abbreviation
ud s l
Access
get/set
Description
If this flag is set, the UDP server is locked to the first client from which it receives a packet. It can send data to, or receive data from, only that client.
If this flag is not set, the udp server receives data from all clients and sends to the last client from which it received a packet.
This flag is useful in stream mode when streaming to only one udp client whose IP is unknown.
Note: The variables udp.server.remote_host and udp.server.remote_port may be used to override this flag. If these variables are set then the udp server replies only to the specified host:port
.
Arguments
1|true|on/0|false|off
where
0
orfalse
oroff
: lock to client disabled1
ortrue
oron
: lock to client enabled
Default
0
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get ud s l
0
Set example
> set ud s l 1
Set OK
udp.server.port
Abbreviation
ud s p
Access
get/set
Description
Default port for UDP server to bind.
Arguments
<port>
Default
3000
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get ud s p
R000006
3000
Set example
> set ud s p 5000
R000008
Set OK
udp.server.remote_host
Abbreviation
ud s h
Access
get/set
Description
Domain or IP address of remote udp client to auto connect. This is used in stream mode when the udp server is configured to auto-start. The stream sends data only to the configured remote host:port. See also udp.server.remote_port.
To disable, set null, i.e. set udp.server.remote_host ""
Note : If the remote_host is not configured, then the UDP server writes to the last client from which it read data (unless the destination address is specified using the udp_server write command).
Arguments
<domain/ip address>
Default
None
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get udp.server.remote_host
mydomain.com
Set example
> set ud c s mydomain.com
Set OK
udp.server.remote_port
Abbreviation
ud s r
Access
get/set
Description
Port of remote UDP client to auto connect. This is used in stream mode when the udp server is configured to auto-start. The stream sends data only to the configured remote host:port. See also udp.server.remote_host.
Note: If the port is 0
then use the UDP server's listening port. See udp.server.port.
Arguments
<port>
Default
3000
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get udp.server.remote_port
Set example
> set ud s r 5000
Set OK