Ethernet
ethernet.auto_start.enabled
Abbreviation
et a e
Access
get/set
Description
Enable/disable network auto-join using the ethernet interface on bootup.
Arguments
0|off|false/1|on|true
Default
0
Platforms
- WGM160P
Properties
Gecko OS Plugin
Get example
> get et a e
R000003
0
Set example
> set et a e true
R000008
Set OK
ethernet.auto_start.retry_delay
Abbreviation
et a d
Access
get/set
Description
The period between auto-join attempts in seconds.
Arguments
0-255
Range: 0 - 255
Default
3
Platforms
- WGM160P
Properties
Gecko OS Plugin
Get example
> get et a d
R000004
10
Set example
> set et a d 5
R000008
Set OK
ethernet.dhcp.cache_enabled
Abbreviation
et d c
Access
get/set
Description
When DHCP caching is enabled, the received DHCP IP address and corresponding lease time is cached to RAM. When the device is rebooted via the reboot command the RAM cache and corresponding timestamp is saved to NVM.
Upon rebooting the saved DHCP IP is restored and the lease time is updated with the amount of time that has elapsed since it was last stored. DHCP IP caching can save a considerable amount of time when re-connecting to the network as the full DHCP sequence is skipped (assuming there is enough time left on the DHCP lease).
See Networking and Security, DHCP Client.
Arguments
1|true|on/0|false|off
where
0
orfalse
oroff
: disabled1
ortrue
oron
: enabled
Default
0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et d c
R000003
0
Set example
> set et d c 0
R000008
Set OK
ethernet.dhcp.enabled
Abbreviation
et d e
Access
get/set
Description
Select whether DHCP is used to automatically obtain an IPv4 IP address on the ethernet interface.
Arguments
0|off|false/1|on|true
Default
1
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get et d e
R000003
1
Set example
> set et d e off
R000008
Set OK
ethernet.dhcp.hostname
Abbreviation
et d h
Access
get/set
Description
Configures the DHCP client's hostname (DHCP option 12) sent to the DHCP server.
Arguments
<hostname>
Default
gecko_os-#
where:
- The character
#
is replaced by the last three digits of the Ethernet MAC address.
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get et d h
R000009
Gecko_OS-#
Set example
> set et d h my_dhcp_client
R000008
Set OK
ethernet.dhcp.timeout
Abbreviation
et d t
Access
get/set
Description
Amount of time in seconds the module waits as a client for an IP from a DHCP server. See ethernet.dhcp.enabled.
Arguments
<timeout_seconds>
Range: 1 - 255
seconds
Default
15
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get et d t
R000004
15
Set example
> set et d t 25
R000008
Set OK
ethernet.link_detected_timeout
Abbreviation
et l
Access
get/set
Description
Time in seconds to wait for for an ethernet link when bringing up the ethernet interface.
Arguments
<seconds>
where:
<seconds>
: Range:1 - 25
Default
7
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et l
R000003
7
Set example
> set et l 10
Set OK
ethernet.link_local.enabled
Abbreviation
et i e
Access
get/set
Description
Enables and disables the link local feature.
The device obtains an IP address using the following sequence:
- IF ethernet.dhcp.enabled == true THEN Attempt DHCP
- IF ethernet.static.ip != 0.0.0.0 THEN Use static IP
- IF ethernet.link_local.enabled == true THEN Attempt Link Local IP (e.g. Auto IP)
If all three steps fail to obtain an IP address then the network_up
sequence fails.
Arguments
1|true|on/0|false|off
where:
1
: enabled0
: disabled
Default
0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get ethernet.link_local.enabled
0
Set example
> set et i e 1
R000008
Set OK
ethernet.link_local.timeout
Abbreviation
et i t
Access
get/set
Description
Configures the maximum time in seconds to obtain an IP via link local protocol.
Arguments
<timeout in seconds>
where:
<timeout in seconds>
is in the range3
to30
Default
20
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get ethernet.link_local.timeout
20
Set example
> set et i t 30
R000008
Set OK
ethernet.mac
Abbreviation
et m
Access
get
Description
Returns the ethernet MAC address.
Arguments
None
Default
varies
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et m
R000019
4C:55:CC:01:23:45
ethernet.multicast.address
Abbreviation
et m a
Access
get
Description
Configure UDP multicast address range.
When the ethernet interface is brought up, it joins the configured multicast group address. When the interface is brought down it leaves the multicast group address.
Notes
The valid multicast group address range is 224.0.0.0 to 239.255.255.255.
0.0.0.0 disables the multicast feature
Multicast is supported only by the UDP client and server. The TCP protocol does not support multicast.
Arguments
<IP address range>
where:
- valid range is
224.0.0.0
to239.255.255.255
0.0.0.0
disables multicast
Default
0.0.0.0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et m a
0.0.0.0
Set example
> set et m a 239.0.0.255
Set OK
ethernet.network.dns
Abbreviation
et n d
Access
get
Description
Return a comma separated list of the DNS server addresses that the Ethernet interface is using.
Note: To set a static DNS address list, use the ethernet.static.dns variable.
Arguments
None
0.0.0.0
indicates no DNS addresses are in use.
Default
0.0.0.0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et n d
10.5.6.1
ethernet.network.gateway
Abbreviation
et n g
Access
get
Description
Returns the Ethernet interface IPv4 gateway IP address resolved by DHCP.
Note: To set a static gateway, use the ethernet.static.gateway variable.
Arguments
None
Default
0.0.0.0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et n g
R000013
192.168.0.1
ethernet.network.ip
Abbreviation
et n i
Access
get
Description
Returns the Ethernet interface IPv4 IP address resolved by DHCP.
Note: To set a static IP address, use the ethernet.static.ip variable.
Arguments
None
Default
0.0.0.0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et n i
R000014
192.168.0.79
ethernet.network.netmask
Abbreviation
et n n
Access
get
Description
Returns the Ethernet interface IPv4 netmask resolved by DHCP.
Note: To set a static netmask, use the ethernet.static.netmask variable.
Arguments
None
Default
0.0.0.0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et n n
R000015
255.255.255.0
ethernet.network.status
Abbreviation
et n s
Access
get
Description
Returns the Ethernet network status:
0
= down1
= connected2
= IP network connected (with a valid IP address)
Arguments
None
Default
0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get et n s
R000003
2
ethernet.network.status_gpio
Abbreviation
et n o
Access
get/set
Description
The GPIO used to indicate network connectivity status. GPIO low = not connected, GPIO high = the default network interface is connected and has an IP address.
See also system.oob.gpio.
Arguments
<GPIO#>
Default
-1
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get et n o
R000004
-1
Set example
> set wl n o 4
R000008
Set OK
ethernet.static.dns
Abbreviation
et s d
Access
get/set
Description
DNS server address if static network settings are used for the Ethernet interface.
Arguments
<[IP address]/[host name]>
Default
8.8.8.8
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get et s d
R000009
8.8.8.8
Set example
> set et s d 8.8.4.4
R000008
Set OK
ethernet.static.gateway
Abbreviation
et s g
Access
get/set
Description
Gateway address if static network settings are used for the Ethernet interface.
Arguments
<IP address>
Default
0.0.0.0
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get et s g
R000009
0.0.0.0
Set example
> set et s g 192.168.0.1
R000008
Set OK
ethernet.static.ip
Abbreviation
et s i
Access
get/set
Description
Local IP address if static network settings are used for the Ethernet interface.
Arguments
<IP address>
Default
0.0.0.0
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get et s i
R000009
0.0.0.0
Set example
> set et s i 192.168.0.2
R000008
Set OK
ethernet.static.netmask
Abbreviation
et s n
Access
get/set
Description
Netmask if static network settings are used for the Ethernet interface.
Arguments
<network mask>
Default
255.255.255.0
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get et s n
R000009
0.0.0.0
Set example
> set et s n 255.255.255.0
R000008
Set OK