mDNS Device Discovery
This example demonstrates how to find the module on the network using a network discovery protocol such as mDNS, LLMNR or Netbios (Gecko OS includes support for all of these protocols). Network discovery enables you to connect with the module using a known domain, rather than a dynamically allocated IP address.
Note : mDNS is not available with some Android apps. See Networking and Security, Network Discovery, Android .
This example demonstrates how to:
- Set up the module to connect to your local network
- Start the Gecko OS mDNS service
- Connect to the module via its mDNS domain
- Advertise an mDNS service
Setup
To run this example follow these steps:
Connect Your Module to the Local Network
To configure mDNS, use a Gecko OS terminal - see Getting Started . Once you have a terminal connected, issue the following Gecko OS command to configure the credentials for the local network:
network_up -s
Enable the mDNS Daemon
Enable mDNS and specify the domain advertised by the module using the following commands:
set mdns.enabled 1
set mdns.name mymodule
Save the mDNS configuration, then restart the network:
save
network_down
network_up
The module automatically starts the network discovery service after connecting to the network.
The response from Gecko OS is similar to the following:
[Associating to mynetwork]
> Obtaining IPv4 address via DHCP
IPv4 address: 10.5.6.59
Starting mDNS
mDNS domain: mymodule.local
[Associated]
Ping the Module using the mDNS Domain
From a command line on a Mac or Windows PC connected to the same local network, send an ICMP ping to the module.
C:\> ping mymodule.local
Pinging mymodule.local [10.5.6.59] with 32 bytes of data:
Reply from 10.5.6.59: bytes=32 time=308ms TTL=128
Reply from 10.5.6.59: bytes=32 time=8ms TTL=128
Reply from 10.5.6.59: bytes=32 time=4ms TTL=128
Reply from 10.5.6.59: bytes=32 time=96ms TTL=128
NOTE
: Some ISPs hijack the
.local
domain which confuses Microsoft Windows, so it may be necessary to omit
.local
from the name on Windows platforms.
If there is no response (on a Windows PC), try sending the ping directly to the module name instead.
C:\> ping mymodule
Pinging mymodule [10.5.6.59] with 32 bytes of data:
Reply from 10.5.6.59: bytes=32 time=33ms TTL=128
Reply from 10.5.6.59: bytes=32 time=17ms TTL=128
Reply from 10.5.6.59: bytes=32 time=5ms TTL=128
Reply from 10.5.6.59: bytes=32 time=29ms TTL=128
Advertise an mDNS Service
This example assumes the network credentials are set up as described in Connect Your Module to the Local Network .
To advertise an mDNS service, you need to start a Gecko OS server. This example uses the HTTP server. To enable the HTTP server, issue the Gecko OS commands:
set http.server.enabled 1
set http.server.api_enabled 1
Advertise the service using the mdns.service variable:
> set md s http "Test Server" "record1=on.record2=off.another=21"
The server name and TXT record name=value pairs are arbitrary in this case. For specific applications, there may be a required naming convention and format for the TXT record information.
Restart the network to begin advertising:
network_down
network_up
The response is similar to the following:
[Associating to My_Network]
In progress
> Obtaining IPv4 address via DHCP
IPv4 address: 10.5.6.82
Starting mDNS
mDNS domain: mymodule.local
Adding mDNS service: Test Server._http._tcp.local
HTTP and REST API server listening on port: 80
[Associated]
Note the line
Adding mDNS service: Test Server._http._tcp.local
.
This means a device capable of browsing for mDNS services will be able to discover your "Test Server" service in the
.local
domain, among the
_http._tcp.
services, and read its name and TXT record for additional information.
If you have a Bonjour browser app you can view the module's advertised services.
To disable advertising of the service, set the server's name to
-1
:
set md s http -1
Now bring the network down and back up:
network_down
network_up
The response is similar to the following:
[2019-01-01 | 06:44:48: Associating to My_Network]
In progress
> Obtaining IPv4 address via DHCP
IPv4 address: 10.5.6.82
Starting mDNS
mDNS domain: nealemodule.local
HTTP and REST API server listening on port: 80
[2019-01-01 | 06:44:51: Associated]
Note that the
Adding mDNS service
line no longer appears.
If you have a Bonjour browser app you can see that the module service is no longer advertised.
Supporting Gecko OS Versions
- Gecko OS 4
Change Log
| Modified | Changes |
|---|---|
| 2019-01-01 | Created |