Multiple TCP Clients
This application uses the Gecko OS TCP client command to open 4 simultaneous TCP connections to a TCP echo server on the internet (Gecko OS actually supports up to 8 simultaneous connections).
The TCP echo server, located on the internet at
test.zentri.com:50007
, simply echoes all received data back to the Gecko OS TCP client. Once each connection is established,
stream_write
is used to send data to each connection stream in turn. With all data sent,
stream_poll
is used to check for received data on connection streams, and
stream_read
is used to read data waiting on a stream.
You will only need one Silicon Labs evaluation board for this example.
Connecting
Let's get started by connecting your board to a Wi-Fi network and opening each of the 4 TCP connection streams in turn. You can simply cut and paste the commands in the following table, but DON'T FORGET to replace your Wi-Fi network name and password for the defaults.
| Gecko OS Commands | Description |
|---|---|
|
|
There is no need to bring up the WLAN network interface prior to opening a TCP connection, the TCP client (just like all commands that need the network) automatically connects to the network if a connection has not already been established.
An example showing what the session looks like if you entered the above commands successfully is shown below. Notice that each new TCP connection is assigned a stream handle, starting at 0 for the first TCP connection.
| Session log when opening 4 TCP client connections |
|---|
|
Check the status of open streams before continuing. Use the stream_list command to get a list of open streams. The number in brackets appended to each line is the local port used for the TCP connection stream.
> stream_list
!# Type Info
#0 TCPC test.zentri.com:50007 (41713)
#1 TCPC test.zentri.com:50007 (46714)
#2 TCPC test.zentri.com:50007 (51715)
#3 TCPC test.zentri.com:50007 (56716)
Writing Data
Writing data to a stream is easy using the stream_write command. Copy and paste the following commands to write data to each open stream.
| Gecko OS Commands | Description |
|---|---|
|
|
Checking for Data
To check for data on any stream (or all streams at once), use the stream_poll command as shown in the following session. If you don't want to poll for data, try assigning a GPIO to a stream to indicate when data is available. The tcp_client command describes how to assign a GPIO.
| Checking for data |
|---|
|
Reading Data
To read available data from any stream, use the stream_read command as shown in the following session.
| Checking for data |
|---|
|
Change Log
| Modified | Changes |
Gecko OS Version
Required |
|---|---|---|
| 2019-01-01 | Created |