UDP Client
udp.client.auto_interface
Abbreviation
ud c i
Access
get/set
Description
Interface to auto-start UDP client connection.
Arguments
default
Default
<default/wlan/softap>
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get udp.client.auto_interface
default
Set example
> set ud c i wlan
Set OK
udp.client.auto_retry
Abbreviation
ud c r
Access
get/set
Description
Enable automatic reconnection if udp.client.auto_start fails.
When enabled, Gecko OS attempts to reconnect every 1.0s until either the network goes down or it successfully connects.
UDP is a connectionless protocol so udp.client.auto_start fails only if udp.client.auto_start cannot resolve the udp.client.remote_host DNS domain. If udp.client.remote_host specifies an IP address, failure to connect is not detected.
Arguments
1|true|on/0|false|off
where
-
0orfalseoroff: auto retry disabled -
1ortrueoron: auto retry enabled
Default
0
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get udp.client.auto_retry
0
Set example
> set ud c r 1
Set OK
udp.client.auto_start
Abbreviation
ud c a
Access
get/set
Description
Enable/disable UDP client auto-start feature. If enabled, UDP client automatically connects to remote server when interface is brought up.
Arguments
1|true|on/0|false|off
where
-
0orfalseoroff: auto retry disabled -
1ortrueoron: auto retry enabled
Default
0
Platforms
- WGM160P
Properties
- network_restart to apply change
Gecko OS Plugin
Get example
> get udp.client.auto_start
0
Set example
> set ud c a 1
Set OK
udp.client.local_port
Abbreviation
ud c l
Access
get/set
Description
Local udp server port.
Arguments
<port>
Default
0
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get udp.client.local_port
0
Set example
> set ud c l 5000
Set OK
udp.client.remote_host
Abbreviation
ud c h
Access
get/set
Description
Domain or IP address of remote udp server to auto connect.
Arguments
<domain/ip address>
Default
None
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get udp.client.remote_host
mydomain.com
Set example
> set ud c h mydomain.com
Set OK
udp.client.remote_port
Abbreviation
ud c p
Access
get/set
Description
Port of remote UDP server to auto connect.
Arguments
<port>
Default
3000
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get udp.client.remote_port
Set example
> set ud c p 5000
Set OK