email.name_address
Abbreviation
em n
Access
get/set
Description
The email name and/or address registered with the SMTP server, used by command API smtp_send command; native API group SMTP API . This is shown as the name and/or email address of the email sender. It may be overridden by the SMTP server.
The name and/or email address is supplied in the standard format for Internet Address Specifications. For further information see Section 3.4, RFC-2822 .
The following get example shows an address only format, and the set example shows an example of a name and address.
See SMTP Client .
For a demonstration, see the Sending a Secure SMTP Email application note.
Arguments
<name_address>
in either of the forms:
-
local-part@domain -
display-name <local-part@domain>
Default
None
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get email.name_address
no.name@example.com
Set example
> set em n "Firstname Lastname <first.last@mydomain.com>"
Set OK
> get em n
Firstname Lastname <first.last@mydomain.com>
email.smtp.host
Abbreviation
em s h
Access
get/set
Description
The SMTP server host (e.g.
smtp.myemail.com
) used by command API
smtp_send
command; native API group
SMTP API
.
See SMTP Client .
Arguments
<host string>
Default
None
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get email.smtp.host
smtp.example.com
Set example
> set em s h smtp.myemail.com
Set OK
email.smtp.password
Abbreviation
em s w
Access
get/set
Description
The SMTP server login password used by command API smtp_send command; native API group SMTP API .
See SMTP Client .
Arguments
<password>
Default
None
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get email.smtp.password
abc123
Set example
> set em s w loooong_SECR3T_password
Set OK
email.smtp.port
Abbreviation
em s p
Access
get/set
Description
The SMTP server port used by command API smtp_send command; native API group SMTP API .
See SMTP Client .
Arguments
<port_number>
Range:
1 - 65535
Default
587
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get email.smtp.port
25
Set example
> set em s p 587
Set OK
email.smtp.username
Abbreviation
em s u
Access
get/set
Description
The SMTP server login username used by the smtp_send command SMTP API . This is optional depending on the SMTP host: email.smtp.host .
See SMTP Client .
Arguments
<user_name>
Default
None
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get email.smtp.username
No Name
Set example
> set email.smtp.user "Firstname Lastname"
Set OK
> get em s u
Firstname Lastname