LESENSE_DecCtrlDesc_TypeDef Struct Reference

LESENSE decoder control descriptor structure.

#include <em_lesense.h>

Data Fields

LESENSE_DecInput_TypeDef decInput
Select input to the LESENSE decoder.
uint32_t initState
Initial state of the LESENSE decoder.
bool chkState
Set to enable decoder to check the present state in addition to the states defined in TCONF.
bool intMap
When set, a transition from state x in decoder will set the interrupt flag CHx.
bool hystPRS0
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.
bool hystPRS1
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.
bool hystPRS2
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.
bool hystIRQ
Set to enable hysteresis in decoder for suppressing the interrupt requests.
bool prsCount
Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.
LESENSE_PRSSel_TypeDef prsChSel0
Select PRS channel input for bit 0 of LESENSE decoder.
LESENSE_PRSSel_TypeDef prsChSel1
Select PRS channel input for bit 1 of LESENSE decoder.
LESENSE_PRSSel_TypeDef prsChSel2
Select PRS channel input for bit 2 of LESENSE decoder.
LESENSE_PRSSel_TypeDef prsChSel3
Select PRS channel input for bit 3 of LESENSE decoder.

LESENSE decoder control descriptor structure.

Field Documentation

◆ decInput

LESENSE_DecInput_TypeDef LESENSE_DecCtrlDesc_TypeDef::decInput

Select input to the LESENSE decoder.

◆ initState

uint32_t LESENSE_DecCtrlDesc_TypeDef::initState

Initial state of the LESENSE decoder.

◆ chkState

bool LESENSE_DecCtrlDesc_TypeDef::chkState

Set to enable decoder to check the present state in addition to the states defined in TCONF.

◆ intMap

bool LESENSE_DecCtrlDesc_TypeDef::intMap

When set, a transition from state x in decoder will set the interrupt flag CHx.

◆ hystPRS0

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.

◆ hystPRS1

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.

◆ hystPRS2

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.

◆ hystIRQ

bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ

Set to enable hysteresis in decoder for suppressing the interrupt requests.

◆ prsCount

bool LESENSE_DecCtrlDesc_TypeDef::prsCount

Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.

◆ prsChSel0

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel0

Select PRS channel input for bit 0 of LESENSE decoder.

◆ prsChSel1

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel1

Select PRS channel input for bit 1 of LESENSE decoder.

◆ prsChSel2

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel2

Select PRS channel input for bit 2 of LESENSE decoder.

◆ prsChSel3

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel3

Select PRS channel input for bit 3 of LESENSE decoder.