ACMP - Analog Comparator

Description

Analog comparator (ACMP) Peripheral API.

The Analog Comparator is used to compare voltage of two analog inputs with a digital output indicating which input voltage is higher. Inputs can either be one of the selectable internal references or from external pins. Response time and current consumption can be configured by altering the current supply to the comparator.

ACMP is available down to EM3 and is able to wake up the system when input signals pass a certain threshold. Use ACMP_IntEnable() to enable an edge interrupt to use this functionality.

This example shows how to use the em_acmp.h API for comparing an input pin to an internal 2.5 V reference voltage.

/* The ACMP is a high-frequency peripheral so we need to enable
* both the HFPER clock and the ACMP0 clock. */
/* Initialize with default settings. */
init. enable = false ;
ACMP_Init (ACMP0, &init);
/* In this example we want to compare an analog input to the 2.5 V
* internal reference. To achieve this we first have to configure the
* VB source which is used for internal reference voltages. */
vbconfig. input = acmpVBInput2V5;
ACMP_VBSetup (ACMP0, &vbconfig);
/* Now we select the two inputs to compare. Here we compare the APORT0XCH0
* input to the internal 2.5V reference that we previously configured. When
* APORT0XCH0 is lower than 2.5 V then the ACMP output is 0 and when
* APORT0XCH0 is is higher than 2.5 V then the ACMP output is 1. */
ACMP_ChannelSet (ACMP0, acmpInputVBDIV, acmpInputAPORT0XCH0);
/* To be able to probe the output we can send the ACMP output to a pin.
* The second argument to this function is the pin location which is
* device dependent. */
ACMP_GPIOSetup (ACMP0, 0, true , false );
/* Finally we enable the ACMP. */
ACMP_Enable (ACMP0);
Note
ACMP can also be used to compare two separate input pins.

ACMP also contains specialized hardware for capacitive sensing. This module contains the ACMP_CapsenseInit() function to initialize ACMP for capacitive sensing and the ACMP_CapsenseChannelSet() function to select the current capsense channel.

For applications that require capacitive sensing it is recommended to use a library, such as cslib, which is provided by Silicon Labs.

Data Structures

struct ACMP_CapsenseInit_TypeDef
Capsense initialization structure.
struct ACMP_Init_TypeDef
ACMP initialization structure.
struct ACMP_VAConfig_TypeDef
VA Configuration structure.
struct ACMP_VBConfig_TypeDef
VB Configuration structure.

Functions

void ACMP_CapsenseInit (ACMP_TypeDef *acmp, const ACMP_CapsenseInit_TypeDef *init)
Set up ACMP for use in capacitive sense applications.
void ACMP_CapsenseChannelSet (ACMP_TypeDef *acmp, ACMP_Channel_TypeDef channel)
Set the ACMP channel used for capacitive sensing.
void ACMP_Disable (ACMP_TypeDef *acmp)
Disable ACMP.
void ACMP_Enable (ACMP_TypeDef *acmp)
Enable ACMP.
void ACMP_Reset (ACMP_TypeDef *acmp)
Reset ACMP to the same state that it was in after a hardware reset.
void ACMP_GPIOSetup (ACMP_TypeDef *acmp, uint32_t location, bool enable, bool invert)
Set up GPIO output from ACMP.
void ACMP_ChannelSet (ACMP_TypeDef *acmp, ACMP_Channel_TypeDef negSel, ACMP_Channel_TypeDef posSel)
Set which channels should be used in ACMP comparisons.
void ACMP_Init (ACMP_TypeDef *acmp, const ACMP_Init_TypeDef *init)
Initialize ACMP.
void ACMP_VASetup (ACMP_TypeDef *acmp, const ACMP_VAConfig_TypeDef *vaconfig)
Set up the VA source.
void ACMP_VBSetup (ACMP_TypeDef *acmp, const ACMP_VBConfig_TypeDef *vbconfig)
Set up the VB Source.
void ACMP_IntClear (ACMP_TypeDef *acmp, uint32_t flags)
Clear one or more pending ACMP interrupts.
void ACMP_IntDisable (ACMP_TypeDef *acmp, uint32_t flags)
Disable one or more ACMP interrupts.
void ACMP_IntEnable (ACMP_TypeDef *acmp, uint32_t flags)
Enable one or more ACMP interrupts.
uint32_t ACMP_IntGet (ACMP_TypeDef *acmp)
Get pending ACMP interrupt flags.
uint32_t ACMP_IntGetEnabled (ACMP_TypeDef *acmp)
Get enabled and pending ACMP interrupt flags.
void ACMP_IntSet (ACMP_TypeDef *acmp, uint32_t flags)
Set one or more pending ACMP interrupts from software.

Macros

#define ACMP_CAPSENSE_INIT_DEFAULT
A default configuration for capacitive sense mode initialization.
#define ACMP_INIT_DEFAULT
Default configuration for ACMP regular initialization.
#define ACMP_VACONFIG_DEFAULT
VA default configuration.
#define ACMP_VBCONFIG_DEFAULT
VB default configuration.

Enumerations

enum ACMP_CapsenseResistor_TypeDef {
acmpResistor0 = _ACMP_INPUTSEL_CSRESSEL_RES0,
acmpResistor1 = _ACMP_INPUTSEL_CSRESSEL_RES1,
acmpResistor2 = _ACMP_INPUTSEL_CSRESSEL_RES2,
acmpResistor3 = _ACMP_INPUTSEL_CSRESSEL_RES3,
acmpResistor4 = _ACMP_INPUTSEL_CSRESSEL_RES4,
acmpResistor5 = _ACMP_INPUTSEL_CSRESSEL_RES5,
acmpResistor6 = _ACMP_INPUTSEL_CSRESSEL_RES6,
acmpResistor7 = _ACMP_INPUTSEL_CSRESSEL_RES7
}
Resistor values used for the internal capacative sense resistor.
enum ACMP_HysteresisLevel_TypeDef {
acmpHysteresisLevel0 = _ACMP_HYSTERESIS0_HYST_HYST0,
acmpHysteresisLevel1 = _ACMP_HYSTERESIS0_HYST_HYST1,
acmpHysteresisLevel2 = _ACMP_HYSTERESIS0_HYST_HYST2,
acmpHysteresisLevel3 = _ACMP_HYSTERESIS0_HYST_HYST3,
acmpHysteresisLevel4 = _ACMP_HYSTERESIS0_HYST_HYST4,
acmpHysteresisLevel5 = _ACMP_HYSTERESIS0_HYST_HYST5,
acmpHysteresisLevel6 = _ACMP_HYSTERESIS0_HYST_HYST6,
acmpHysteresisLevel7 = _ACMP_HYSTERESIS0_HYST_HYST7,
acmpHysteresisLevel8 = _ACMP_HYSTERESIS0_HYST_HYST8,
acmpHysteresisLevel9 = _ACMP_HYSTERESIS0_HYST_HYST9,
acmpHysteresisLevel10 = _ACMP_HYSTERESIS0_HYST_HYST10,
acmpHysteresisLevel11 = _ACMP_HYSTERESIS0_HYST_HYST11,
acmpHysteresisLevel12 = _ACMP_HYSTERESIS0_HYST_HYST12,
acmpHysteresisLevel13 = _ACMP_HYSTERESIS0_HYST_HYST13,
acmpHysteresisLevel14 = _ACMP_HYSTERESIS0_HYST_HYST14,
acmpHysteresisLevel15 = _ACMP_HYSTERESIS0_HYST_HYST15
}
Hysteresis level.
enum ACMP_InputRange_TypeDef {
acmpInputRangeFull = _ACMP_CTRL_INPUTRANGE_FULL,
acmpInputRangeHigh = _ACMP_CTRL_INPUTRANGE_GTVDDDIV2,
acmpInputRangeLow = _ACMP_CTRL_INPUTRANGE_LTVDDDIV2
}
Adjust ACMP performance for a given input voltage range.
enum ACMP_PowerSource_TypeDef {
acmpPowerSourceAvdd = _ACMP_CTRL_PWRSEL_AVDD,
acmpPowerSourceDvdd = _ACMP_CTRL_PWRSEL_DVDD,
acmpPowerSourceIOVdd0 = _ACMP_CTRL_PWRSEL_IOVDD0,
acmpPowerSourceIOVdd1 = _ACMP_CTRL_PWRSEL_IOVDD1
}
ACMP Power source.
enum ACMP_Accuracy_TypeDef {
acmpAccuracyLow = _ACMP_CTRL_ACCURACY_LOW,
acmpAccuracyHigh = _ACMP_CTRL_ACCURACY_HIGH
}
ACMP accuracy mode.
enum ACMP_VAInput_TypeDef {
acmpVAInputVDD = _ACMP_INPUTSEL_VASEL_VDD,
acmpVAInputAPORT2YCH0 = _ACMP_INPUTSEL_VASEL_APORT2YCH0,
acmpVAInputAPORT2YCH2 = _ACMP_INPUTSEL_VASEL_APORT2YCH2,
acmpVAInputAPORT2YCH4 = _ACMP_INPUTSEL_VASEL_APORT2YCH4,
acmpVAInputAPORT2YCH6 = _ACMP_INPUTSEL_VASEL_APORT2YCH6,
acmpVAInputAPORT2YCH8 = _ACMP_INPUTSEL_VASEL_APORT2YCH8,
acmpVAInputAPORT2YCH10 = _ACMP_INPUTSEL_VASEL_APORT2YCH10,
acmpVAInputAPORT2YCH12 = _ACMP_INPUTSEL_VASEL_APORT2YCH12,
acmpVAInputAPORT2YCH14 = _ACMP_INPUTSEL_VASEL_APORT2YCH14,
acmpVAInputAPORT2YCH16 = _ACMP_INPUTSEL_VASEL_APORT2YCH16,
acmpVAInputAPORT2YCH18 = _ACMP_INPUTSEL_VASEL_APORT2YCH18,
acmpVAInputAPORT2YCH20 = _ACMP_INPUTSEL_VASEL_APORT2YCH20,
acmpVAInputAPORT2YCH22 = _ACMP_INPUTSEL_VASEL_APORT2YCH22,
acmpVAInputAPORT2YCH24 = _ACMP_INPUTSEL_VASEL_APORT2YCH24,
acmpVAInputAPORT2YCH26 = _ACMP_INPUTSEL_VASEL_APORT2YCH26,
acmpVAInputAPORT2YCH28 = _ACMP_INPUTSEL_VASEL_APORT2YCH28,
acmpVAInputAPORT2YCH30 = _ACMP_INPUTSEL_VASEL_APORT2YCH30,
acmpVAInputAPORT1XCH0 = _ACMP_INPUTSEL_VASEL_APORT1XCH0,
acmpVAInputAPORT1YCH1 = _ACMP_INPUTSEL_VASEL_APORT1YCH1,
acmpVAInputAPORT1XCH2 = _ACMP_INPUTSEL_VASEL_APORT1XCH2,
acmpVAInputAPORT1YCH3 = _ACMP_INPUTSEL_VASEL_APORT1YCH3,
acmpVAInputAPORT1XCH4 = _ACMP_INPUTSEL_VASEL_APORT1XCH4,
acmpVAInputAPORT1YCH5 = _ACMP_INPUTSEL_VASEL_APORT1YCH5,
acmpVAInputAPORT1XCH6 = _ACMP_INPUTSEL_VASEL_APORT1XCH6,
acmpVAInputAPORT1YCH7 = _ACMP_INPUTSEL_VASEL_APORT1YCH7,
acmpVAInputAPORT1XCH8 = _ACMP_INPUTSEL_VASEL_APORT1XCH8,
acmpVAInputAPORT1YCH9 = _ACMP_INPUTSEL_VASEL_APORT1YCH9,
acmpVAInputAPORT1XCH10 = _ACMP_INPUTSEL_VASEL_APORT1XCH10,
acmpVAInputAPORT1YCH11 = _ACMP_INPUTSEL_VASEL_APORT1YCH11,
acmpVAInputAPORT1XCH12 = _ACMP_INPUTSEL_VASEL_APORT1XCH12,
acmpVAInputAPORT1YCH13 = _ACMP_INPUTSEL_VASEL_APORT1YCH13,
acmpVAInputAPORT1XCH14 = _ACMP_INPUTSEL_VASEL_APORT1XCH14,
acmpVAInputAPORT1YCH15 = _ACMP_INPUTSEL_VASEL_APORT1YCH15,
acmpVAInputAPORT1XCH16 = _ACMP_INPUTSEL_VASEL_APORT1XCH16,
acmpVAInputAPORT1YCH17 = _ACMP_INPUTSEL_VASEL_APORT1YCH17,
acmpVAInputAPORT1XCH18 = _ACMP_INPUTSEL_VASEL_APORT1XCH18,
acmpVAInputAPORT1YCH19 = _ACMP_INPUTSEL_VASEL_APORT1YCH19,
acmpVAInputAPORT1XCH20 = _ACMP_INPUTSEL_VASEL_APORT1XCH20,
acmpVAInputAPORT1YCH21 = _ACMP_INPUTSEL_VASEL_APORT1YCH21,
acmpVAInputAPORT1XCH22 = _ACMP_INPUTSEL_VASEL_APORT1XCH22,
acmpVAInputAPORT1YCH23 = _ACMP_INPUTSEL_VASEL_APORT1YCH23,
acmpVAInputAPORT1XCH24 = _ACMP_INPUTSEL_VASEL_APORT1XCH24,
acmpVAInputAPORT1YCH25 = _ACMP_INPUTSEL_VASEL_APORT1YCH25,
acmpVAInputAPORT1XCH26 = _ACMP_INPUTSEL_VASEL_APORT1XCH26,
acmpVAInputAPORT1YCH27 = _ACMP_INPUTSEL_VASEL_APORT1YCH27,
acmpVAInputAPORT1XCH28 = _ACMP_INPUTSEL_VASEL_APORT1XCH28,
acmpVAInputAPORT1YCH29 = _ACMP_INPUTSEL_VASEL_APORT1YCH29,
acmpVAInputAPORT1XCH30 = _ACMP_INPUTSEL_VASEL_APORT1XCH30,
acmpVAInputAPORT1YCH31 = _ACMP_INPUTSEL_VASEL_APORT1YCH31
}
ACMP input to the VA divider.
enum ACMP_VBInput_TypeDef {
acmpVBInput1V25 = _ACMP_INPUTSEL_VBSEL_1V25,
acmpVBInput2V5 = _ACMP_INPUTSEL_VBSEL_2V5
}
ACMP input to the VB divider.
enum ACMP_VLPInput_Typedef {
acmpVLPInputVADIV = _ACMP_INPUTSEL_VLPSEL_VADIV,
acmpVLPInputVBDIV = _ACMP_INPUTSEL_VLPSEL_VBDIV
}
ACMP Low-Power Input Selection.
enum ACMP_Channel_TypeDef {
acmpInputAPORT0XCH0 = _ACMP_INPUTSEL_POSSEL_APORT0XCH0,
acmpInputAPORT0XCH1 = _ACMP_INPUTSEL_POSSEL_APORT0XCH1,
acmpInputAPORT0XCH2 = _ACMP_INPUTSEL_POSSEL_APORT0XCH2,
acmpInputAPORT0XCH3 = _ACMP_INPUTSEL_POSSEL_APORT0XCH3,
acmpInputAPORT0XCH4 = _ACMP_INPUTSEL_POSSEL_APORT0XCH4,
acmpInputAPORT0XCH5 = _ACMP_INPUTSEL_POSSEL_APORT0XCH5,
acmpInputAPORT0XCH6 = _ACMP_INPUTSEL_POSSEL_APORT0XCH6,
acmpInputAPORT0XCH7 = _ACMP_INPUTSEL_POSSEL_APORT0XCH7,
acmpInputAPORT0XCH8 = _ACMP_INPUTSEL_POSSEL_APORT0XCH8,
acmpInputAPORT0XCH9 = _ACMP_INPUTSEL_POSSEL_APORT0XCH9,
acmpInputAPORT0XCH10 = _ACMP_INPUTSEL_POSSEL_APORT0XCH10,
acmpInputAPORT0XCH11 = _ACMP_INPUTSEL_POSSEL_APORT0XCH11,
acmpInputAPORT0XCH12 = _ACMP_INPUTSEL_POSSEL_APORT0XCH12,
acmpInputAPORT0XCH13 = _ACMP_INPUTSEL_POSSEL_APORT0XCH13,
acmpInputAPORT0XCH14 = _ACMP_INPUTSEL_POSSEL_APORT0XCH14,
acmpInputAPORT0XCH15 = _ACMP_INPUTSEL_POSSEL_APORT0XCH15,
acmpInputAPORT0YCH0 = _ACMP_INPUTSEL_POSSEL_APORT0YCH0,
acmpInputAPORT0YCH1 = _ACMP_INPUTSEL_POSSEL_APORT0YCH1,
acmpInputAPORT0YCH2 = _ACMP_INPUTSEL_POSSEL_APORT0YCH2,
acmpInputAPORT0YCH3 = _ACMP_INPUTSEL_POSSEL_APORT0YCH3,
acmpInputAPORT0YCH4 = _ACMP_INPUTSEL_POSSEL_APORT0YCH4,
acmpInputAPORT0YCH5 = _ACMP_INPUTSEL_POSSEL_APORT0YCH5,
acmpInputAPORT0YCH6 = _ACMP_INPUTSEL_POSSEL_APORT0YCH6,
acmpInputAPORT0YCH7 = _ACMP_INPUTSEL_POSSEL_APORT0YCH7,
acmpInputAPORT0YCH8 = _ACMP_INPUTSEL_POSSEL_APORT0YCH8,
acmpInputAPORT0YCH9 = _ACMP_INPUTSEL_POSSEL_APORT0YCH9,
acmpInputAPORT0YCH10 = _ACMP_INPUTSEL_POSSEL_APORT0YCH10,
acmpInputAPORT0YCH11 = _ACMP_INPUTSEL_POSSEL_APORT0YCH11,
acmpInputAPORT0YCH12 = _ACMP_INPUTSEL_POSSEL_APORT0YCH12,
acmpInputAPORT0YCH13 = _ACMP_INPUTSEL_POSSEL_APORT0YCH13,
acmpInputAPORT0YCH14 = _ACMP_INPUTSEL_POSSEL_APORT0YCH14,
acmpInputAPORT0YCH15 = _ACMP_INPUTSEL_POSSEL_APORT0YCH15,
acmpInputAPORT1XCH0 = _ACMP_INPUTSEL_POSSEL_APORT1XCH0,
acmpInputAPORT1YCH1 = _ACMP_INPUTSEL_POSSEL_APORT1YCH1,
acmpInputAPORT1XCH2 = _ACMP_INPUTSEL_POSSEL_APORT1XCH2,
acmpInputAPORT1YCH3 = _ACMP_INPUTSEL_POSSEL_APORT1YCH3,
acmpInputAPORT1XCH4 = _ACMP_INPUTSEL_POSSEL_APORT1XCH4,
acmpInputAPORT1YCH5 = _ACMP_INPUTSEL_POSSEL_APORT1YCH5,
acmpInputAPORT1XCH6 = _ACMP_INPUTSEL_POSSEL_APORT1XCH6,
acmpInputAPORT1YCH7 = _ACMP_INPUTSEL_POSSEL_APORT1YCH7,
acmpInputAPORT1XCH8 = _ACMP_INPUTSEL_POSSEL_APORT1XCH8,
acmpInputAPORT1YCH9 = _ACMP_INPUTSEL_POSSEL_APORT1YCH9,
acmpInputAPORT1XCH10 = _ACMP_INPUTSEL_POSSEL_APORT1XCH10,
acmpInputAPORT1YCH11 = _ACMP_INPUTSEL_POSSEL_APORT1YCH11,
acmpInputAPORT1XCH12 = _ACMP_INPUTSEL_POSSEL_APORT1XCH12,
acmpInputAPORT1YCH13 = _ACMP_INPUTSEL_POSSEL_APORT1YCH13,
acmpInputAPORT1XCH14 = _ACMP_INPUTSEL_POSSEL_APORT1XCH14,
acmpInputAPORT1YCH15 = _ACMP_INPUTSEL_POSSEL_APORT1YCH15,
acmpInputAPORT1XCH16 = _ACMP_INPUTSEL_POSSEL_APORT1XCH16,
acmpInputAPORT1YCH17 = _ACMP_INPUTSEL_POSSEL_APORT1YCH17,
acmpInputAPORT1XCH18 = _ACMP_INPUTSEL_POSSEL_APORT1XCH18,
acmpInputAPORT1YCH19 = _ACMP_INPUTSEL_POSSEL_APORT1YCH19,
acmpInputAPORT1XCH20 = _ACMP_INPUTSEL_POSSEL_APORT1XCH20,
acmpInputAPORT1YCH21 = _ACMP_INPUTSEL_POSSEL_APORT1YCH21,
acmpInputAPORT1XCH22 = _ACMP_INPUTSEL_POSSEL_APORT1XCH22,
acmpInputAPORT1YCH23 = _ACMP_INPUTSEL_POSSEL_APORT1YCH23,
acmpInputAPORT1XCH24 = _ACMP_INPUTSEL_POSSEL_APORT1XCH24,
acmpInputAPORT1YCH25 = _ACMP_INPUTSEL_POSSEL_APORT1YCH25,
acmpInputAPORT1XCH26 = _ACMP_INPUTSEL_POSSEL_APORT1XCH26,
acmpInputAPORT1YCH27 = _ACMP_INPUTSEL_POSSEL_APORT1YCH27,
acmpInputAPORT1XCH28 = _ACMP_INPUTSEL_POSSEL_APORT1XCH28,
acmpInputAPORT1YCH29 = _ACMP_INPUTSEL_POSSEL_APORT1YCH29,
acmpInputAPORT1XCH30 = _ACMP_INPUTSEL_POSSEL_APORT1XCH30,
acmpInputAPORT1YCH31 = _ACMP_INPUTSEL_POSSEL_APORT1YCH31,
acmpInputAPORT2YCH0 = _ACMP_INPUTSEL_POSSEL_APORT2YCH0,
acmpInputAPORT2XCH1 = _ACMP_INPUTSEL_POSSEL_APORT2XCH1,
acmpInputAPORT2YCH2 = _ACMP_INPUTSEL_POSSEL_APORT2YCH2,
acmpInputAPORT2XCH3 = _ACMP_INPUTSEL_POSSEL_APORT2XCH3,
acmpInputAPORT2YCH4 = _ACMP_INPUTSEL_POSSEL_APORT2YCH4,
acmpInputAPORT2XCH5 = _ACMP_INPUTSEL_POSSEL_APORT2XCH5,
acmpInputAPORT2YCH6 = _ACMP_INPUTSEL_POSSEL_APORT2YCH6,
acmpInputAPORT2XCH7 = _ACMP_INPUTSEL_POSSEL_APORT2XCH7,
acmpInputAPORT2YCH8 = _ACMP_INPUTSEL_POSSEL_APORT2YCH8,
acmpInputAPORT2XCH9 = _ACMP_INPUTSEL_POSSEL_APORT2XCH9,
acmpInputAPORT2YCH10 = _ACMP_INPUTSEL_POSSEL_APORT2YCH10,
acmpInputAPORT2XCH11 = _ACMP_INPUTSEL_POSSEL_APORT2XCH11,
acmpInputAPORT2YCH12 = _ACMP_INPUTSEL_POSSEL_APORT2YCH12,
acmpInputAPORT2XCH13 = _ACMP_INPUTSEL_POSSEL_APORT2XCH13,
acmpInputAPORT2YCH14 = _ACMP_INPUTSEL_POSSEL_APORT2YCH14,
acmpInputAPORT2XCH15 = _ACMP_INPUTSEL_POSSEL_APORT2XCH15,
acmpInputAPORT2YCH16 = _ACMP_INPUTSEL_POSSEL_APORT2YCH16,
acmpInputAPORT2XCH17 = _ACMP_INPUTSEL_POSSEL_APORT2XCH17,
acmpInputAPORT2YCH18 = _ACMP_INPUTSEL_POSSEL_APORT2YCH18,
acmpInputAPORT2XCH19 = _ACMP_INPUTSEL_POSSEL_APORT2XCH19,
acmpInputAPORT2YCH20 = _ACMP_INPUTSEL_POSSEL_APORT2YCH20,
acmpInputAPORT2XCH21 = _ACMP_INPUTSEL_POSSEL_APORT2XCH21,
acmpInputAPORT2YCH22 = _ACMP_INPUTSEL_POSSEL_APORT2YCH22,
acmpInputAPORT2XCH23 = _ACMP_INPUTSEL_POSSEL_APORT2XCH23,
acmpInputAPORT2YCH24 = _ACMP_INPUTSEL_POSSEL_APORT2YCH24,
acmpInputAPORT2XCH25 = _ACMP_INPUTSEL_POSSEL_APORT2XCH25,
acmpInputAPORT2YCH26 = _ACMP_INPUTSEL_POSSEL_APORT2YCH26,
acmpInputAPORT2XCH27 = _ACMP_INPUTSEL_POSSEL_APORT2XCH27,
acmpInputAPORT2YCH28 = _ACMP_INPUTSEL_POSSEL_APORT2YCH28,
acmpInputAPORT2XCH29 = _ACMP_INPUTSEL_POSSEL_APORT2XCH29,
acmpInputAPORT2YCH30 = _ACMP_INPUTSEL_POSSEL_APORT2YCH30,
acmpInputAPORT2XCH31 = _ACMP_INPUTSEL_POSSEL_APORT2XCH31,
acmpInputAPORT3XCH0 = _ACMP_INPUTSEL_POSSEL_APORT3XCH0,
acmpInputAPORT3YCH1 = _ACMP_INPUTSEL_POSSEL_APORT3YCH1,
acmpInputAPORT3XCH2 = _ACMP_INPUTSEL_POSSEL_APORT3XCH2,
acmpInputAPORT3YCH3 = _ACMP_INPUTSEL_POSSEL_APORT3YCH3,
acmpInputAPORT3XCH4 = _ACMP_INPUTSEL_POSSEL_APORT3XCH4,
acmpInputAPORT3YCH5 = _ACMP_INPUTSEL_POSSEL_APORT3YCH5,
acmpInputAPORT3XCH6 = _ACMP_INPUTSEL_POSSEL_APORT3XCH6,
acmpInputAPORT3YCH7 = _ACMP_INPUTSEL_POSSEL_APORT3YCH7,
acmpInputAPORT3XCH8 = _ACMP_INPUTSEL_POSSEL_APORT3XCH8,
acmpInputAPORT3YCH9 = _ACMP_INPUTSEL_POSSEL_APORT3YCH9,
acmpInputAPORT3XCH10 = _ACMP_INPUTSEL_POSSEL_APORT3XCH10,
acmpInputAPORT3YCH11 = _ACMP_INPUTSEL_POSSEL_APORT3YCH11,
acmpInputAPORT3XCH12 = _ACMP_INPUTSEL_POSSEL_APORT3XCH12,
acmpInputAPORT3YCH13 = _ACMP_INPUTSEL_POSSEL_APORT3YCH13,
acmpInputAPORT3XCH14 = _ACMP_INPUTSEL_POSSEL_APORT3XCH14,
acmpInputAPORT3YCH15 = _ACMP_INPUTSEL_POSSEL_APORT3YCH15,
acmpInputAPORT3XCH16 = _ACMP_INPUTSEL_POSSEL_APORT3XCH16,
acmpInputAPORT3YCH17 = _ACMP_INPUTSEL_POSSEL_APORT3YCH17,
acmpInputAPORT3XCH18 = _ACMP_INPUTSEL_POSSEL_APORT3XCH18,
acmpInputAPORT3YCH19 = _ACMP_INPUTSEL_POSSEL_APORT3YCH19,
acmpInputAPORT3XCH20 = _ACMP_INPUTSEL_POSSEL_APORT3XCH20,
acmpInputAPORT3YCH21 = _ACMP_INPUTSEL_POSSEL_APORT3YCH21,
acmpInputAPORT3XCH22 = _ACMP_INPUTSEL_POSSEL_APORT3XCH22,
acmpInputAPORT3YCH23 = _ACMP_INPUTSEL_POSSEL_APORT3YCH23,
acmpInputAPORT3XCH24 = _ACMP_INPUTSEL_POSSEL_APORT3XCH24,
acmpInputAPORT3YCH25 = _ACMP_INPUTSEL_POSSEL_APORT3YCH25,
acmpInputAPORT3XCH26 = _ACMP_INPUTSEL_POSSEL_APORT3XCH26,
acmpInputAPORT3YCH27 = _ACMP_INPUTSEL_POSSEL_APORT3YCH27,
acmpInputAPORT3XCH28 = _ACMP_INPUTSEL_POSSEL_APORT3XCH28,
acmpInputAPORT3YCH29 = _ACMP_INPUTSEL_POSSEL_APORT3YCH29,
acmpInputAPORT3XCH30 = _ACMP_INPUTSEL_POSSEL_APORT3XCH30,
acmpInputAPORT3YCH31 = _ACMP_INPUTSEL_POSSEL_APORT3YCH31,
acmpInputAPORT4YCH0 = _ACMP_INPUTSEL_POSSEL_APORT4YCH0,
acmpInputAPORT4XCH1 = _ACMP_INPUTSEL_POSSEL_APORT4XCH1,
acmpInputAPORT4YCH2 = _ACMP_INPUTSEL_POSSEL_APORT4YCH2,
acmpInputAPORT4XCH3 = _ACMP_INPUTSEL_POSSEL_APORT4XCH3,
acmpInputAPORT4YCH4 = _ACMP_INPUTSEL_POSSEL_APORT4YCH4,
acmpInputAPORT4XCH5 = _ACMP_INPUTSEL_POSSEL_APORT4XCH5,
acmpInputAPORT4YCH6 = _ACMP_INPUTSEL_POSSEL_APORT4YCH6,
acmpInputAPORT4XCH7 = _ACMP_INPUTSEL_POSSEL_APORT4XCH7,
acmpInputAPORT4YCH8 = _ACMP_INPUTSEL_POSSEL_APORT4YCH8,
acmpInputAPORT4XCH9 = _ACMP_INPUTSEL_POSSEL_APORT4XCH9,
acmpInputAPORT4YCH10 = _ACMP_INPUTSEL_POSSEL_APORT4YCH10,
acmpInputAPORT4XCH11 = _ACMP_INPUTSEL_POSSEL_APORT4XCH11,
acmpInputAPORT4YCH12 = _ACMP_INPUTSEL_POSSEL_APORT4YCH12,
acmpInputAPORT4XCH13 = _ACMP_INPUTSEL_POSSEL_APORT4XCH13,
acmpInputAPORT4YCH16 = _ACMP_INPUTSEL_POSSEL_APORT4YCH16,
acmpInputAPORT4XCH17 = _ACMP_INPUTSEL_POSSEL_APORT4XCH17,
acmpInputAPORT4YCH18 = _ACMP_INPUTSEL_POSSEL_APORT4YCH18,
acmpInputAPORT4XCH19 = _ACMP_INPUTSEL_POSSEL_APORT4XCH19,
acmpInputAPORT4YCH20 = _ACMP_INPUTSEL_POSSEL_APORT4YCH20,
acmpInputAPORT4XCH21 = _ACMP_INPUTSEL_POSSEL_APORT4XCH21,
acmpInputAPORT4YCH22 = _ACMP_INPUTSEL_POSSEL_APORT4YCH22,
acmpInputAPORT4XCH23 = _ACMP_INPUTSEL_POSSEL_APORT4XCH23,
acmpInputAPORT4YCH24 = _ACMP_INPUTSEL_POSSEL_APORT4YCH24,
acmpInputAPORT4XCH25 = _ACMP_INPUTSEL_POSSEL_APORT4XCH25,
acmpInputAPORT4YCH26 = _ACMP_INPUTSEL_POSSEL_APORT4YCH26,
acmpInputAPORT4XCH27 = _ACMP_INPUTSEL_POSSEL_APORT4XCH27,
acmpInputAPORT4YCH28 = _ACMP_INPUTSEL_POSSEL_APORT4YCH28,
acmpInputAPORT4XCH29 = _ACMP_INPUTSEL_POSSEL_APORT4XCH29,
acmpInputAPORT4YCH30 = _ACMP_INPUTSEL_POSSEL_APORT4YCH30,
acmpInputAPORT4YCH14 = _ACMP_INPUTSEL_POSSEL_APORT4YCH14,
acmpInputAPORT4XCH15 = _ACMP_INPUTSEL_POSSEL_APORT4XCH15,
acmpInputAPORT4XCH31 = _ACMP_INPUTSEL_POSSEL_APORT4XCH31,
acmpInputVLP = _ACMP_INPUTSEL_POSSEL_VLP,
acmpInputVBDIV = _ACMP_INPUTSEL_POSSEL_VBDIV,
acmpInputVADIV = _ACMP_INPUTSEL_POSSEL_VADIV,
acmpInputVDD = _ACMP_INPUTSEL_POSSEL_VDD,
acmpInputVSS = _ACMP_INPUTSEL_POSSEL_VSS
}
ACMP Input Selection.

Function Documentation

◆ ACMP_CapsenseInit()

void ACMP_CapsenseInit ( ACMP_TypeDef * acmp,
const ACMP_CapsenseInit_TypeDef * init
)

Set up ACMP for use in capacitive sense applications.

This function sets up ACMP for use in capacitive sense applications. To use the capacitive sense functionality in the ACMP, use the PRS output of the ACMP module to count the number of oscillations in the capacitive sense circuit (possibly using a TIMER).

Note
A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] init A pointer to the initialization structure used to configure ACMP for capacitive sensing operation.

◆ ACMP_CapsenseChannelSet()

void ACMP_CapsenseChannelSet ( ACMP_TypeDef * acmp,
ACMP_Channel_TypeDef channel
)

Set the ACMP channel used for capacitive sensing.

Note
A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] channel The ACMP channel to use for capacitive sensing (Possel).

◆ ACMP_Disable()

void ACMP_Disable ( ACMP_TypeDef * acmp )

Disable ACMP.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.

◆ ACMP_Enable()

void ACMP_Enable ( ACMP_TypeDef * acmp )

Enable ACMP.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.

◆ ACMP_Reset()

void ACMP_Reset ( ACMP_TypeDef * acmp )

Reset ACMP to the same state that it was in after a hardware reset.

Note
The GPIO ACMP ROUTE register is NOT reset by this function to allow for centralized setup of this feature.
The peripheral may be enabled and disabled during reset.
Parameters
[in] acmp A pointer to the ACMP peripheral register block.

◆ ACMP_GPIOSetup()

void ACMP_GPIOSetup ( ACMP_TypeDef * acmp,
uint32_t location,
bool enable,
bool invert
)

Set up GPIO output from ACMP.

Note
GPIO must be enabled in the CMU before this function call, i.e.,
CMU_ClockEnable(cmuClock_GPIO, true); 
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
location The pin location to use. See the data sheet for location to pin mappings.
enable Enable or disable pin output.
invert Invert output.

◆ ACMP_ChannelSet()

void ACMP_ChannelSet ( ACMP_TypeDef * acmp,
ACMP_Channel_TypeDef negSel,
ACMP_Channel_TypeDef posSel
)

Set which channels should be used in ACMP comparisons.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
negSel A channel to use on the negative input to the ACMP.
posSel A channel to use on the positive input to the ACMP.

◆ ACMP_Init()

void ACMP_Init ( ACMP_TypeDef * acmp,
const ACMP_Init_TypeDef * init
)

Initialize ACMP.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] init A pointer to the initialization structure used to configure ACMP.

◆ ACMP_VASetup()

void ACMP_VASetup ( ACMP_TypeDef * acmp,
const ACMP_VAConfig_TypeDef * vaconfig
)

Set up the VA source.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] vaconfig A pointer to the structure used to configure the VA source. This structure contains the input source and the 2 divider values.

◆ ACMP_VBSetup()

void ACMP_VBSetup ( ACMP_TypeDef * acmp,
const ACMP_VBConfig_TypeDef * vbconfig
)

Set up the VB Source.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] vbconfig A pointer to the structure used to configure the VB source. This structure contains the input source and the 2 divider values.

◆ ACMP_IntClear()

void ACMP_IntClear ( ACMP_TypeDef * acmp,
uint32_t flags
)
inline

Clear one or more pending ACMP interrupts.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] flags Pending ACMP interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFC_EDGE or ACMP_IFC_WARMUP.

◆ ACMP_IntDisable()

void ACMP_IntDisable ( ACMP_TypeDef * acmp,
uint32_t flags
)
inline

Disable one or more ACMP interrupts.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] flags ACMP interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP.

◆ ACMP_IntEnable()

void ACMP_IntEnable ( ACMP_TypeDef * acmp,
uint32_t flags
)
inline

Enable one or more ACMP interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using ACMP_IntClear() prior to enabling if a pending interrupt should be ignored.
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] flags ACMP interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP.

◆ ACMP_IntGet()

uint32_t ACMP_IntGet ( ACMP_TypeDef * acmp )
inline

Get pending ACMP interrupt flags.

Note
This function does not clear event bits.
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
Returns
Pending ACMP interrupt sources. A bitwise logic OR combination of valid interrupt flags for the ACMP module. The pending interrupt sources can be, for instance, ACMP_IF_EDGE or ACMP_IF_WARMUP.

◆ ACMP_IntGetEnabled()

uint32_t ACMP_IntGetEnabled ( ACMP_TypeDef * acmp )
inline

Get enabled and pending ACMP interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
Note
This function does not clear interrupt flags.
Returns
Pending and enabled ACMP interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in ACMPx_IEN_nnn register (ACMPx_IEN_nnn) and
  • the OR combination of valid interrupt flags of the ACMP module (ACMPx_IF_nnn).

◆ ACMP_IntSet()

void ACMP_IntSet ( ACMP_TypeDef * acmp,
uint32_t flags
)
inline

Set one or more pending ACMP interrupts from software.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] flags ACMP interrupt sources to set as pending. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFS_EDGE or ACMP_IFS_WARMUP.

Macro Definition Documentation

◆ ACMP_CAPSENSE_INIT_DEFAULT

#define ACMP_CAPSENSE_INIT_DEFAULT
Value:
{ \
false, /* Don't use fullBias to lower power consumption. */ \
0x20, /* Using biasProg value of 0x20 (32). */ \
acmpHysteresisLevel8, /* Use hysteresis level 8 when ACMP output is 0. */ \
acmpHysteresisLevel8, /* Use hysteresis level 8 when ACMP output is 1. */ \
acmpResistor5, /* Use internal resistor value 5. */ \
0x30, /* VDD level high. */ \
0x10, /* VDD level low. */ \
true /* Enable after initialization. */ \
}

A default configuration for capacitive sense mode initialization.

◆ ACMP_INIT_DEFAULT

#define ACMP_INIT_DEFAULT
Value:
{ \
false, /* fullBias */ \
0x7, /* biasProg */ \
false, /* No interrupt on falling edge. */ \
false, /* No interrupt on rising edge. */ \
acmpInputRangeFull, /* Input range from 0 to VDD. */ \
acmpAccuracyLow, /* Low accuracy, less current usage. */ \
acmpPowerSourceAvdd, /* Use the AVDD supply. */ \
acmpHysteresisLevel5, /* Use hysteresis level 5 when output is 0 */ \
acmpHysteresisLevel5, /* Use hysteresis level 5 when output is 1 */ \
acmpVLPInputVADIV, /* Use VADIV as the VLP input source. */ \
false, /* Output 0 when ACMP is inactive. */ \
true /* Enable after init. */ \
}

Default configuration for ACMP regular initialization.

◆ ACMP_VACONFIG_DEFAULT

#define ACMP_VACONFIG_DEFAULT
Value:
{ \
acmpVAInputVDD, /* Use VDD as VA voltage input source. */ \
63, /* No division of the VA source when ACMP output is 0. */ \
63, /* No division of the VA source when ACMP output is 1. */ \
}

VA default configuration.

◆ ACMP_VBCONFIG_DEFAULT

#define ACMP_VBCONFIG_DEFAULT
Value:
{ \
acmpVBInput1V25, /* Use 1.25 V as VB voltage input source. */ \
63, /* No division of the VB source when ACMP output is 0. */ \
63, /* No division of the VB source when ACMP output is 1. */ \
}

VB default configuration.

Enumeration Type Documentation

◆ ACMP_CapsenseResistor_TypeDef

Resistor values used for the internal capacative sense resistor.

See data sheet for your device for details on each resistor value.

Enumerator
acmpResistor0

Resistor value 0.

acmpResistor1

Resistor value 1.

acmpResistor2

Resistor value 2.

acmpResistor3

Resistor value 3.

acmpResistor4

Resistor value 4.

acmpResistor5

Resistor value 5.

acmpResistor6

Resistor value 6.

acmpResistor7

Resistor value 7.

◆ ACMP_HysteresisLevel_TypeDef

Hysteresis level.

See data sheet for your device for details on each level.

Enumerator
acmpHysteresisLevel0

Hysteresis level 0.

acmpHysteresisLevel1

Hysteresis level 1.

acmpHysteresisLevel2

Hysteresis level 2.

acmpHysteresisLevel3

Hysteresis level 3.

acmpHysteresisLevel4

Hysteresis level 4.

acmpHysteresisLevel5

Hysteresis level 5.

acmpHysteresisLevel6

Hysteresis level 6.

acmpHysteresisLevel7

Hysteresis level 7.

acmpHysteresisLevel8

Hysteresis level 8.

acmpHysteresisLevel9

Hysteresis level 9.

acmpHysteresisLevel10

Hysteresis level 10.

acmpHysteresisLevel11

Hysteresis level 11.

acmpHysteresisLevel12

Hysteresis level 12.

acmpHysteresisLevel13

Hysteresis level 13.

acmpHysteresisLevel14

Hysteresis level 14.

acmpHysteresisLevel15

Hysteresis level 15.

◆ ACMP_InputRange_TypeDef

Adjust ACMP performance for a given input voltage range.

Enumerator
acmpInputRangeFull

Input can be from 0 to VDD.

acmpInputRangeHigh

Input will always be greater than VDD/2.

acmpInputRangeLow

Input will always be less than VDD/2.

◆ ACMP_PowerSource_TypeDef

ACMP Power source.

Enumerator
acmpPowerSourceAvdd

Power ACMP using the AVDD supply.

acmpPowerSourceDvdd

Power ACMP using the DVDD supply.

acmpPowerSourceIOVdd0

Power ACMP using the IOVDD/IOVDD0 supply.

acmpPowerSourceIOVdd1

Power ACMP using the IOVDD1 supply (if the part has two I/O voltages).

◆ ACMP_Accuracy_TypeDef

ACMP accuracy mode.

Enumerator
acmpAccuracyLow

Low-accuracy mode which consumes less current.

acmpAccuracyHigh

High-accuracy mode which consumes more current.

◆ ACMP_VAInput_TypeDef

ACMP input to the VA divider.

This enumeration is used to select the input for the VA Divider.

◆ ACMP_VBInput_TypeDef

ACMP input to the VB divider.

This enumeration is used to select the input for the VB divider.

◆ ACMP_VLPInput_Typedef

ACMP Low-Power Input Selection.

◆ ACMP_Channel_TypeDef

ACMP Input Selection.