EMU_VmonHystInit_TypeDef Struct Reference
VMON Hysteresis initialization structure.
#include <em_emu.h>
Data Fields | |
EMU_VmonChannel_TypeDef | channel |
VMON channel to configure. | |
int | riseThreshold |
Rising threshold (mV). | |
int | fallThreshold |
Falling threshold (mV). | |
bool | riseWakeup |
Wake up from EM4H on rising edge. | |
bool | fallWakeup |
Wake up from EM4H on falling edge. | |
bool | enable |
Enable VMON channel. | |
VMON Hysteresis initialization structure.
Field Documentation
◆ channel
EMU_VmonChannel_TypeDef EMU_VmonHystInit_TypeDef::channel |
VMON channel to configure.
◆ riseThreshold
int EMU_VmonHystInit_TypeDef::riseThreshold |
Rising threshold (mV).
◆ fallThreshold
int EMU_VmonHystInit_TypeDef::fallThreshold |
Falling threshold (mV).
◆ riseWakeup
bool EMU_VmonHystInit_TypeDef::riseWakeup |
Wake up from EM4H on rising edge.
◆ fallWakeup
bool EMU_VmonHystInit_TypeDef::fallWakeup |
Wake up from EM4H on falling edge.
◆ enable
bool EMU_VmonHystInit_TypeDef::enable |
Enable VMON channel.