PCNT - Pulse Counter

Description

Pulse Counter (PCNT) Peripheral API.

This module contains functions to control the PCNT peripheral of Silicon Labs 32-bit MCUs and SoCs. The PCNT decodes incoming pulses. The module has a quadrature mode which may be used to decode the speed and direction of a mechanical shaft.

Data Structures

struct PCNT_Init_TypeDef
Initialization structure.

Functions

uint32_t PCNT_CounterGet (PCNT_TypeDef *pcnt)
Default configuration for PCNT initialization structure.
void PCNT_CounterReset (PCNT_TypeDef *pcnt)
Reset PCNT counters and TOP register.
void PCNT_CounterTopSet (PCNT_TypeDef *pcnt, uint32_t count, uint32_t top)
Set the counter and top values.
void PCNT_CounterSet (PCNT_TypeDef *pcnt, uint32_t count)
Set counter value.
void PCNT_Enable (PCNT_TypeDef *pcnt, PCNT_Mode_TypeDef mode)
Set PCNT operational mode.
bool PCNT_IsEnabled (PCNT_TypeDef *pcnt)
Returns if the PCNT module is enabled or not.
void PCNT_FreezeEnable (PCNT_TypeDef *pcnt, bool enable)
PCNT register synchronization freeze control.
void PCNT_Init (PCNT_TypeDef *pcnt, const PCNT_Init_TypeDef *init)
Initialize the pulse counter.
void PCNT_IntClear (PCNT_TypeDef *pcnt, uint32_t flags)
Clear one or more pending PCNT interrupts.
void PCNT_IntDisable (PCNT_TypeDef *pcnt, uint32_t flags)
Disable one or more PCNT interrupts.
void PCNT_IntEnable (PCNT_TypeDef *pcnt, uint32_t flags)
Enable one or more PCNT interrupts.
uint32_t PCNT_IntGet (PCNT_TypeDef *pcnt)
Get pending PCNT interrupt flags.
uint32_t PCNT_IntGetEnabled (PCNT_TypeDef *pcnt)
Get enabled and pending PCNT interrupt flags.
void PCNT_IntSet (PCNT_TypeDef *pcnt, uint32_t flags)
Set one or more pending PCNT interrupts from SW.
void PCNT_Reset (PCNT_TypeDef *pcnt)
Reset PCNT to the same state that it was in after a hardware reset.
uint32_t PCNT_TopBufferGet (PCNT_TypeDef *pcnt)
Get pulse counter top buffer value.
void PCNT_TopBufferSet (PCNT_TypeDef *pcnt, uint32_t val)
Set top buffer value.
uint32_t PCNT_TopGet (PCNT_TypeDef *pcnt)
Get pulse counter top value.
void PCNT_TopSet (PCNT_TypeDef *pcnt, uint32_t val)
Set the top value.
void PCNT_Sync (PCNT_TypeDef *pcnt, uint32_t mask)
Wait for an ongoing sync of register(s) to low-frequency domain to complete.

Macros

#define PCNT0_CNT_SIZE (8) /* PCNT0 counter is 8 bits. */
PCNT0 Counter register size.
#define PCNT1_CNT_SIZE (8) /* PCNT1 counter is 8 bits. */
PCNT1 Counter register size.
#define PCNT2_CNT_SIZE (8) /* PCNT2 counter is 8 bits. */
PCNT2 Counter register size.
#define PCNT_MODE_DISABLE 0xFF
#define PCNT_CNT_EVEN_NONE 0xFF
#define DEFAULT_DEBUG_HALT
Default configuration for PCNT initialization structure.
#define DEFAULT_MODE pcntModeDisable , /* Disabled by default. */
#define DEFAULT_HYST
#define DEFAULT_CDIR
#define DEFAULT_CNTEV
#define DEFAULT_AUXCNTEV
#define DEFAULT_PRS_CH
#define PCNT_INIT_DEFAULT

Enumerations

enum PCNT_Mode_TypeDef {
pcntModeDisable = _PCNT_CTRL_MODE_DISABLE,
pcntModeOvsSingle = _PCNT_CTRL_MODE_OVSSINGLE,
pcntModeExtSingle = _PCNT_CTRL_MODE_EXTCLKSINGLE,
pcntModeExtQuad = _PCNT_CTRL_MODE_EXTCLKQUAD
}
Mode selection.

Function Documentation

◆ PCNT_CounterGet()

uint32_t PCNT_CounterGet ( PCNT_TypeDef * pcnt )
inline

Default configuration for PCNT initialization structure.

Get pulse counter value.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Current pulse counter value.

◆ PCNT_CounterReset()

void PCNT_CounterReset ( PCNT_TypeDef * pcnt )

Reset PCNT counters and TOP register.

Note
Notice that special SYNCBUSY handling is not applicable for the RSTEN bit of the control register, so we don't need to wait for it when only modifying RSTEN. (It would mean undefined wait time if clocked by an external clock.) The SYNCBUSY bit will however be set, leading to a synchronization in the LF domain, with, in reality, no changes.
Parameters
[in] pcnt A pointer to the PCNT peripheral register block.

◆ PCNT_CounterTopSet()

void PCNT_CounterTopSet ( PCNT_TypeDef * pcnt,
uint32_t count,
uint32_t top
)

Set the counter and top values.

The pulse counter is disabled while changing these values and reenabled (if originally enabled) when values have been set.

Note
This function will stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module, since stall time may be undefined. The counter should normally only be set when operating in (or about to enable) pcntModeOvsSingle mode.
Parameters
[in] pcnt A pointer to the PCNT peripheral register block.
[in] count A value to set in the counter register.
[in] top A value to set in the top register.

◆ PCNT_CounterSet()

void PCNT_CounterSet ( PCNT_TypeDef * pcnt,
uint32_t count
)
inline

Set counter value.

Pulse counter is disabled while changing counter value, and re-enabled (if originally enabled) when counter value has been set.

Note
This function will stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when using an external clock to clock the PCNT module since stall time may be undefined in that case. The counter should normally only be set when operating in (or about to enable) pcntModeOvsSingle mode.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] count Value to set in counter register.

◆ PCNT_Enable()

void PCNT_Enable ( PCNT_TypeDef * pcnt,
PCNT_Mode_TypeDef mode
)

Set PCNT operational mode.

Notice that this function does not do any configuration. Setting operational mode is normally only required after initialization is done, and if not done as part of initialization or if requiring to disable/reenable pulse counter.

Note
This function may stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module, since stall time may be undefined.
Parameters
[in] pcnt A pointer to the PCNT peripheral register block.
[in] mode An operational mode to use for PCNT.

◆ PCNT_IsEnabled()

bool PCNT_IsEnabled ( PCNT_TypeDef * pcnt )

Returns if the PCNT module is enabled or not.

Notice that this function does not do any configuration.

Parameters
[in] pcnt A pointer to the PCNT peripheral register block.
[out] isEnabled Returns TRUE if the module is enabled.

◆ PCNT_FreezeEnable()

void PCNT_FreezeEnable ( PCNT_TypeDef * pcnt,
bool enable
)

PCNT register synchronization freeze control.

Some PCNT registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several registers to be modified before passing them to the LF domain simultaneously, which takes place when the freeze mode is disabled.

Note
When enabling freeze mode, this function will wait for all current ongoing PCNT synchronization to the LF domain to complete (normally synchronization will not be in progress). However, for this reason, when using freeze mode, modifications of registers requiring the LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling.
Parameters
[in] pcnt A pointer to the PCNT peripheral register block.
[in] enable
  • True - enable freeze, modified registers are not propagated to the LF domain.
  • False - disables freeze, modified registers are propagated to LF domain.

◆ PCNT_Init()

void PCNT_Init ( PCNT_TypeDef * pcnt,
const PCNT_Init_TypeDef * init
)

Initialize the pulse counter.

This function will configure the pulse counter. The clock selection is configured as follows, depending on operational mode:

Notice that the LFACLK must be enabled in all modes, since some basic setup is done with this clock even if the external pin clock usage mode is chosen. The pulse counter clock for the selected instance must also be enabled prior to initialization.

Notice that pins used by the PCNT module must be properly configured by the user explicitly through setting the ROUTE register for the PCNT to work as intended.

Writing to CNT will not occur in external clock modes (EXTCLKQUAD and EXTCLKSINGLE) because the external clock rate is unknown. The user should handle it manually depending on the application.

TOPB is written for all modes but in external clock mode it will take 3 external clock cycles to sync to TOP.

Note
Initializing requires synchronization into the low-frequency domain. This may cause a delay.
Parameters
[in] pcnt A pointer to the PCNT peripheral register block.
[in] init A pointer to the initialization structure.

◆ PCNT_IntClear()

void PCNT_IntClear ( PCNT_TypeDef * pcnt,
uint32_t flags
)
inline

Clear one or more pending PCNT interrupts.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] flags Pending PCNT interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the PCNT module (PCNT_IF_nnn).

◆ PCNT_IntDisable()

void PCNT_IntDisable ( PCNT_TypeDef * pcnt,
uint32_t flags
)
inline

Disable one or more PCNT interrupts.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] flags PCNT interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for PCNT module (PCNT_IF_nnn).

◆ PCNT_IntEnable()

void PCNT_IntEnable ( PCNT_TypeDef * pcnt,
uint32_t flags
)
inline

Enable one or more PCNT interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using PCNT_IntClear() prior to enabling the interrupt.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] flags PCNT interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for PCNT module (PCNT_IF_nnn).

◆ PCNT_IntGet()

uint32_t PCNT_IntGet ( PCNT_TypeDef * pcnt )
inline

Get pending PCNT interrupt flags.

Note
The event bits are not cleared by the use of this function.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
PCNT interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for PCNT module (PCNT_IF_nnn).

◆ PCNT_IntGetEnabled()

uint32_t PCNT_IntGetEnabled ( PCNT_TypeDef * pcnt )
inline

Get enabled and pending PCNT interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
The event bits are not cleared by the use of this function.
Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Pending and enabled PCNT interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in PCNT_IEN_nnn register (PCNT_IEN_nnn) and
  • the OR combination of valid interrupt flags of the PCNT module (PCNT_IF_nnn).

◆ PCNT_IntSet()

void PCNT_IntSet ( PCNT_TypeDef * pcnt,
uint32_t flags
)
inline

Set one or more pending PCNT interrupts from SW.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
[in] flags PCNT interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for PCNT module (PCNT_IF_nnn).

◆ PCNT_Reset()

void PCNT_Reset ( PCNT_TypeDef * pcnt )

Reset PCNT to the same state that it was in after a hardware reset.

Notice the LFACLK must be enabled, since some basic reset is done with this clock. The pulse counter clock for the selected instance must also be enabled prior to initialization.

Note
The ROUTE register is NOT reset by this function to allow for centralized setup of this feature.
Parameters
[in] pcnt A pointer to the PCNT peripheral register block.

◆ PCNT_TopBufferGet()

uint32_t PCNT_TopBufferGet ( PCNT_TypeDef * pcnt )
inline

Get pulse counter top buffer value.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Current pulse counter top buffer value.

◆ PCNT_TopBufferSet()

void PCNT_TopBufferSet ( PCNT_TypeDef * pcnt,
uint32_t val
)

Set top buffer value.

Note
This function may stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module since stall time may be undefined.
Parameters
[in] pcnt A pointer to the PCNT peripheral register block.
[in] val A value to set in the top buffer register.

◆ PCNT_TopGet()

uint32_t PCNT_TopGet ( PCNT_TypeDef * pcnt )
inline

Get pulse counter top value.

Parameters
[in] pcnt Pointer to PCNT peripheral register block.
Returns
Current pulse counter top value.

◆ PCNT_TopSet()

void PCNT_TopSet ( PCNT_TypeDef * pcnt,
uint32_t val
)

Set the top value.

Note
This function will stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module since stall time may be undefined.
Parameters
[in] pcnt A pointer to the PCNT peripheral register block.
[in] val A value to set in the top register.

◆ PCNT_Sync()

void PCNT_Sync ( PCNT_TypeDef * pcnt,
uint32_t mask
)
inline

Wait for an ongoing sync of register(s) to low-frequency domain to complete.

Parameters
[in] pcnt A pointer to the PCNT peripheral register block.
[in] mask A bitmask corresponding to SYNCBUSY register defined bits indicating registers that must complete any ongoing synchronization.

Macro Definition Documentation

◆ PCNT0_CNT_SIZE

#define PCNT0_CNT_SIZE   (8) /* PCNT0 counter is 8 bits. */

PCNT0 Counter register size.

◆ PCNT1_CNT_SIZE

#define PCNT1_CNT_SIZE   (8) /* PCNT1 counter is 8 bits. */

PCNT1 Counter register size.

◆ PCNT2_CNT_SIZE

#define PCNT2_CNT_SIZE   (8) /* PCNT2 counter is 8 bits. */

PCNT2 Counter register size.

◆ DEFAULT_DEBUG_HALT

#define DEFAULT_DEBUG_HALT

Default configuration for PCNT initialization structure.

◆ PCNT_INIT_DEFAULT

#define PCNT_INIT_DEFAULT
Value:
{ \
DEFAULT_MODE /* Default mode. */ \
_PCNT_CNT_RESETVALUE, /* Default counter HW reset value. */ \
_PCNT_TOP_RESETVALUE, /* Default counter HW reset value. */ \
false, /* Use positive edge. */ \
false, /* Up-counting. */ \
false, /* Filter disabled. */ \
DEFAULT_DEBUG_HALT /* Debug Halt enabled. */ \
DEFAULT_HYST /* Default Hysteresis. */ \
DEFAULT_CDIR /* Default CNTDIR. */ \
DEFAULT_CNTEV /* Faults CNTEV. */ \
DEFAULT_AUXCNTEV /* Default AUXCNTEV. */ \
DEFAULT_PRS_CH /* PRS channel 0 selected as S0IN. */ \
DEFAULT_PRS_CH /* PRS channel 0 selected as S1IN. */ \
}

Enumeration Type Documentation

◆ PCNT_Mode_TypeDef

Mode selection.

Enumerator
pcntModeDisable

Disable pulse counter.

pcntModeOvsSingle

Single input LFACLK oversampling mode (available in EM0-EM2).

pcntModeExtSingle

Externally clocked single input counter mode (available in EM0-EM3).

pcntModeExtQuad

Externally clocked quadrature decoder mode (available in EM0-EM3).