Board APIs
The board APIs controls features specific to the Silicon Labs kit boards, like GPIO controlled power to external sensors. The board control API consists of both runtime functions to control the state and compile time configuration done through config headers which are editable by the user. During device initialization the configuration header settings are then applied by the board component itself.
Thunderboard Sense 2 (BRD4166A) Support
Thunderboard Sense 2 has several I 2 C buses connected to the various sensors that are all connected to the EFR32. The BRD4166A support component provides functions to route pin connections of an I2C peripheral to the various I 2 C buses. This allows time multiplexed access to several I 2 C buses using only one I2C peripheral.