Token Manager
Description
Routines for working with tokens.
Introduction
The token system stores such non-volatile information as the manufacturing ID, channel number, transmit power, and various pieces of information that the application needs to be persistent between device power cycles. The token system is design to abstract implementation details and simplify interacting with differing non-volatile systems. The majority of tokens are stored in NVM3 or Simulated EEPROM (both use Flash) where they can be rewritten. Manufacturing tokens are stored in dedicated regions of flash and are not designed to be rewritten.
By default the Token Manager pulls in the NVM3 component for storage. If the SimEE1 or SimEE2 component is added into the project along side the Token Manager, then SimEE1 or SimEE2 will be used for storage. If the Sim EEPROM 2 to NVM3 Upgrade component is added to the project along side the Token Manager, then the upgrade will run at startup to transition as much stored data as possible into NVM3 format. When using the upgrade component don't include NVM3 or SimEE2 components. Once an upgrade is run, it would be possible to use stock Token Manager since Token Manager defaults to NVM3.
Functions |
|
| Ecode_t | sl_token_init (void) |
|
Initialize the Token Manager.
|
|
| Ecode_t | sl_token_get_data (uint32_t token, uint32_t index, void *data, uint32_t length) |
|
Read the data stored in the specified data or manufacturing token.
|
|
| Ecode_t | sl_token_get_pointer_or_data (uint32_t token, uint8_t index, void *pointer, uint32_t length) |
|
Read the data stored in or return a pointer to the specified data or manufacturing token.
|
|
| Ecode_t | sl_token_set_data (uint32_t token, uint32_t index, void *data, uint32_t length) |
|
Writes the data to the specified token.
|
|
| Ecode_t | sl_token_increment_counter (uint32_t token) |
|
Increments the value of a counter token.
|
|
| Ecode_t | sl_token_get_manufacturing_data (uint32_t token, uint32_t index, void *data, uint32_t length) |
|
Read the data associated with the specified manufacturing token.
|
|
| Ecode_t | sl_token_set_manufacturing_data (uint32_t token, void *data, uint32_t length) |
|
Writes data to a manufacturing token.
|
|
Function Documentation
◆ sl_token_init()
| Ecode_t sl_token_init | ( | void |
|
) |
Initialize the Token Manager.
- Note
- This function must be called before any other sl_token functions. If it does not return success, the other sl_token functions will not work.
- Returns
- 0 if successful. Error code otherwise.
◆ sl_token_get_data()
| Ecode_t sl_token_get_data | ( | uint32_t |
token,
|
| uint32_t |
index,
|
||
| void * |
data,
|
||
| uint32_t |
length
|
||
| ) |
Read the data stored in the specified data or manufacturing token.
- Parameters
-
tokenThe NVM3KEY or SimEE CREATOR define for the token. indexThe index to access in the indexed token. dataA pointer to where the token data should be placed. lengthThe size of the token data in number of bytes.
- Returns
- 0 if successful. Error code otherwise.
◆ sl_token_get_pointer_or_data()
| Ecode_t sl_token_get_pointer_or_data | ( | uint32_t |
token,
|
| uint8_t |
index,
|
||
| void * |
pointer,
|
||
| uint32_t |
length
|
||
| ) |
Read the data stored in or return a pointer to the specified data or manufacturing token.
- Parameters
-
tokenThe NVM3KEY or SimEE CREATOR define for the token. indexThe index to access in the indexed token. pointerA pointer to where the token data should be placed or a pointer to where the data can be read. lengthThe size of the token data in number of bytes.
- Returns
- 0 if successful. Error code otherwise.
◆ sl_token_set_data()
| Ecode_t sl_token_set_data | ( | uint32_t |
token,
|
| uint32_t |
index,
|
||
| void * |
data,
|
||
| uint32_t |
length
|
||
| ) |
Writes the data to the specified token.
- Parameters
-
tokenThe NVM3KEY or SimEE CREATOR define for the token. indexThe index to access in the indexed token. dataA pointer to the data being written. lengthThe size of the token data in number of bytes.
- Returns
- 0 if successful. Error code otherwise.
◆ sl_token_increment_counter()
| Ecode_t sl_token_increment_counter | ( | uint32_t |
token
|
) |
Increments the value of a counter token.
This call does not support manufacturing tokens.
- Parameters
-
tokenThe NVM3KEY or SimEE CREATOR define for the token.
- Returns
- 0 if successful. Error code otherwise.
◆ sl_token_get_manufacturing_data()
| Ecode_t sl_token_get_manufacturing_data | ( | uint32_t |
token,
|
| uint32_t |
index,
|
||
| void * |
data,
|
||
| uint32_t |
length
|
||
| ) |
Read the data associated with the specified manufacturing token.
- Parameters
-
tokenThe NVM3KEY or SimEE CREATOR define for the token. indexThe index to access in the indexed token. dataA pointer to where the token data should be placed. lengthThe size of the token data in number of bytes.
- Returns
- 0 if successful. Error code otherwise.
◆ sl_token_set_manufacturing_data()
| Ecode_t sl_token_set_manufacturing_data | ( | uint32_t |
token,
|
| void * |
data,
|
||
| uint32_t |
length
|
||
| ) |
Writes data to a manufacturing token.
- Note
- Only manufacturing token values that have not been written since the last erase can be written. For areas of flash that cannot be erased by user code, those manufacturing tokens are effectively write-once.
- Parameters
-
tokenThe NVM3KEY or SimEE CREATOR define for the token. dataA pointer to the data being written. lengthThe size of the token data in number of bytes.
- Returns
- 0 if successful. Error code otherwise.