LFXO Initialization
Description
Initialize the LFXO oscillator.
Configure the low frequency crystal oscillator using settings in the configuration header
sl_device_init_lfxo_config.h
.
The precision of the oscillator can be indicated using the configuration option
SL_DEVICE_INIT_LFXO_PRECISION
. This is used by certain wireless stacks to optimize wakeup time for scheduled events (such as Bluetooth advertising).
Functions |
|
| sl_status_t | sl_device_init_lfxo (void) |
|
Initialize LFXO.
|
|
Function Documentation
◆ sl_device_init_lfxo()
| sl_status_t sl_device_init_lfxo | ( | void |
|
) |
Initialize LFXO.
Configure the low frequency crystal oscillator using settings in the configuration header
sl_device_init_lfxo_config.h
.
The precision of the oscillator can be indicated using the configuration option
SL_DEVICE_INIT_LFXO_PRECISION
. This is used by certain wireless stacks to optimize wakeup time for scheduled events (such as Bluetooth advertising).
- Returns
- Status code
- Return values
-
SL_STATUS_OKLFXO initialized successfully