sl_se_cert_size_type_t Struct Reference

Certificate size data structure.

#include <sl_se_manager_types.h>

Data Fields

uint32_t batch_id_size
size in bytes of the Batch certificate
uint32_t se_id_size
size in bytes of the SE ID certificate
uint32_t host_id_size
size in bytes of the Host ID certificate

Certificate size data structure.

Field Documentation

batch_id_size

uint32_t sl_se_cert_size_type_t::batch_id_size

size in bytes of the Batch certificate

se_id_size

uint32_t sl_se_cert_size_type_t::se_id_size

size in bytes of the SE ID certificate

host_id_size

uint32_t sl_se_cert_size_type_t::host_id_size

size in bytes of the Host ID certificate