__BMP_DataType Struct Reference
BMP Data type structure to hold information about the bmp data returned.
#include <bmp.h>
Data Fields |
|
| uint16_t | bitsPerPixel |
|
Color depth of the data returned from function.
|
|
| uint32_t | compressionType |
|
Compression type.
|
|
| uint32_t | size |
|
Byte length of returned data.
|
|
| uint32_t | endOfRow |
|
Marks whether this data is at the end of the current row.
|
|
BMP Data type structure to hold information about the bmp data returned.
Field Documentation
◆ bitsPerPixel
| uint16_t __BMP_DataType::bitsPerPixel |
Color depth of the data returned from function.
◆ compressionType
| uint32_t __BMP_DataType::compressionType |
Compression type.
◆ size
| uint32_t __BMP_DataType::size |
Byte length of returned data.
◆ endOfRow
| uint32_t __BMP_DataType::endOfRow |
Marks whether this data is at the end of the current row.
endOfRow == 1, if end of row is reached. endOfRow == 0, if there is still unread data left in the row