GLIB BMP
Description
Bitmap Support.
Data Structures |
|
| struct | BMP_Header |
|
BMP Module header structure.
|
|
| struct | __BMP_Palette |
|
BMP palette structure to hold palette pointer and size.
|
|
| struct | __BMP_DataType |
|
BMP Data type structure to hold information about the bmp data returned.
|
|
Functions |
|
| struct __BMP_Header | __attribute__ ((__packed__)) |
| EMSTATUS | BMP_init (uint8_t *palette, uint32_t paletteSize, EMSTATUS(*fp)(uint8_t buffer[], uint32_t bufLength, uint32_t bytesToRead)) |
|
Initializes BMP Module.
|
|
| EMSTATUS | BMP_reset (void) |
|
Makes the module ready for new bmp file.
|
|
| EMSTATUS | BMP_readRgbData (uint8_t buffer[], uint32_t bufLength, uint32_t *pixelsRead) |
|
Reads in data from BMP file and fills buffer with RGB values.
|
|
| EMSTATUS | BMP_readRawData (BMP_DataType *dataType, uint8_t buffer[], uint32_t bufLength) |
|
Fills buffer with raw data from BMP file.
|
|
| int32_t | BMP_getWidth (void) |
|
Get width of BMP image in pixels.
|
|
| int32_t | BMP_getHeight (void) |
|
Get height of BMP image in pixels.
|
|
| int16_t | BMP_getBitsPerPixel (void) |
|
Get color depth (bits per pixel)
|
|
| int32_t | BMP_getCompressionType (void) |
|
Get compression type.
|
|
| int32_t | BMP_getImageDataSize (void) |
|
Get imageDataSize in bytes.
|
|
| int32_t | BMP_getDataOffset (void) |
|
Get the offset, i.e.
|
|
| int32_t | BMP_getFileSize (void) |
|
Get the fileSize in bytes.
|
|
Macros |
|
| #define | ECODE_BMP_BASE 0x00000000 |
|
BMP base error code.
|
|
| #define | BMP_OK 0x00000000 |
|
Successful call.
|
|
| #define | BMP_END_OF_FILE |
|
End of file has been reached.
|
|
| #define | BMP_ERROR_IO ( ECODE_BMP_BASE | 0x0001) |
|
General IO error.
|
|
| #define | BMP_ERROR_HEADER_SIZE_MISMATCH ( ECODE_BMP_BASE | 0x0002) |
|
BMP_Header size in bytes is different from BMP_HEADER_SIZE.
|
|
| #define | BMP_ERROR_ENDIAN_MISMATCH ( ECODE_BMP_BASE | 0x0003) |
|
Endian mismatch.
|
|
| #define | BMP_ERROR_FILE_NOT_SUPPORTED ( ECODE_BMP_BASE | 0x0004) |
|
BMP file is not supported.
|
|
| #define | BMP_ERROR_FILE_INVALID ( ECODE_BMP_BASE | 0x0005) |
|
BMP "file" is not a BMP file.
|
|
| #define | BMP_ERROR_INVALID_ARGUMENT ( ECODE_BMP_BASE | 0x0006) |
|
Argument passed to function is invalid.
|
|
| #define | BMP_ERROR_MODULE_NOT_INITIALIZED ( ECODE_BMP_BASE | 0x0007) |
|
BMP module is not initialized.
|
|
| #define | BMP_ERROR_INVALID_PALETTE_SIZE ( ECODE_BMP_BASE | 0x0008) |
|
Invalid palette size.
|
|
| #define | BMP_ERROR_FILE_NOT_RESET ( ECODE_BMP_BASE | 0x0009) |
|
File not reset.
|
|
| #define | BMP_ERROR_END_OF_FILE ( ECODE_BMP_BASE | 0x0010) |
|
End of bmp file is reached.
|
|
| #define | BMP_ERROR_BUFFER_TOO_SMALL ( ECODE_BMP_BASE | 0x0020) |
|
Buffer provided is too small.
|
|
| #define | BMP_ERROR_PALETTE_NOT_READ ( ECODE_BMP_BASE | 0x0030) |
|
Bmp palette is not read.
|
|
| #define | BMP_PALETTE_8BIT_SIZE (256 * 4) |
|
Palette size in bytes.
|
|
| #define | BMP_HEADER_SIZE (54) |
|
BMP Header Size in bytes.
|
|
| #define | BMP_LOCAL_CACHE_LIMIT (3) |
|
BMP Local cache limit.
|
|
| #define | RLE8_COMPRESSION (1) |
|
Use RLE8 compression.
|
|
| #define | NO_COMPRESSION (0) |
|
Use no compression.
|
|
| #define | BMP_LOCAL_CACHE_SIZE (BMP_CONFIG_LOCAL_CACHE_SIZE) |
|
BMP Local cache size.
|
|
Function Documentation
◆ BMP_init()
| EMSTATUS BMP_init | ( | uint8_t * |
palette,
|
| uint32_t |
paletteSize,
|
||
| EMSTATUS(*)(uint8_t buffer[], uint32_t bufLength, uint32_t bytesToRead) |
fp
|
||
| ) |
Initializes BMP Module.
Support:
- 24-bit Uncompressed.
- 8-bit Uncompressed.
- 8-bit RLE compressed.
- Parameters
-
paletteData buffer to hold palette. Required for 8bpp BMPs. paletteSizeSize of palette in bytes. If BMP is 8-bit, this potentially has to be 256 * 4 bytes. If the user knows that he only loads BMPs with N bytes, he can pass in paletteSize = N. Otherwise this value should be 256 * 4 = 1024 bytes to ensure that the palette is big enough for all 8-bits BMPs. fpFunction pointer that is used to read in bytes from BMP file. The function has to return an EMSTATUS and have the following parameter list (uint32_t buffer[], uint32_t bufLength, uint32_t bytesToRead). The function should fill (buffer) with (bytesToRead) bytes from the beginning. If it succeds it has to return BMP_OK, otherwise it should return BMP_ERROR_IO. When the function returns it should be ready to read from where it left off.
- Returns
- Returns BMP_OK on success, or else error code.
◆ BMP_reset()
| EMSTATUS BMP_reset | ( |
|
) |
Makes the module ready for new bmp file.
Reads in header from file, and checks if the provided bmp file is valid and supported. It reads in palette if BMP file is 8bpp. Uses function pointer set in BMP_init() .
- Returns
- Returns BMP_OK on success, or else error code
◆ BMP_readRgbData()
| EMSTATUS BMP_readRgbData | ( | uint8_t |
buffer[],
|
| uint32_t |
bufLength,
|
||
| uint32_t * |
pixelsRead
|
||
| ) |
Reads in data from BMP file and fills buffer with RGB values.
This function terminates either when the buffer is full, end of row is reached or end of file is reached.
- Parameters
-
bufferBuffer to hold RGB values. bufLengthBuffer length in bytes. pixelsReadPointer to a uint32_t which holds how many bytes that are read.
- Returns
-
- Returns BMP_OK on success
- Returns BMP_ERROR_END_OF_FILE if end of file is reached
- Returns error code otherwise.
◆ BMP_readRawData()
| EMSTATUS BMP_readRawData | ( | BMP_DataType * |
dataType,
|
| uint8_t |
buffer[],
|
||
| uint32_t |
bufLength
|
||
| ) |
Fills buffer with raw data from BMP file.
- If data is 24bit: Buffer is filled with RGB values till its full or end of row is reached.
- If data is 8bit: Buffer is filled with palette indicies till its full or end of row is reached.
- If data is RLE8: Buffer is filled with number of pixels, followed by palette indicies like this (N is number of pixels, P is palette index) buffer = { N P N P ... }.
- Data is 24bpp if dataType.bitsPerPixel == 24 and dataType.compressionType == NO_COMPRESSION.
- Data is 8bpp if dataType.bitsPerPixel == 8 and dataType.compressionType == NO_COMPRESSION.
- Data is RLE8 if dataType.bitsPerPixel == 8 and dataType.compressionType == RLE8_COMPRESSION.
- Parameters
-
dataTypeData type struct which holds information about the data returned bufferBuffer to be filled with raw data bufLengthLength of buffer
- Returns
- Returns BMP_OK on success, or else error code
◆ BMP_getWidth()
| int32_t BMP_getWidth | ( |
|
) |
Get width of BMP image in pixels.
- Returns
- Returns width of image, or -1 on error
◆ BMP_getHeight()
| int32_t BMP_getHeight | ( |
|
) |
Get height of BMP image in pixels.
- Returns
- Returns height, or -1 on error
◆ BMP_getBitsPerPixel()
| int16_t BMP_getBitsPerPixel | ( |
|
) |
Get color depth (bits per pixel)
- Returns
- Returns bitsPerPixel, or -1 on error
◆ BMP_getCompressionType()
| int32_t BMP_getCompressionType | ( |
|
) |
Get compression type.
0 - No compression 1 - RLE 8bpp 2 - RLE 4bpp
- Returns
- Returns compressionType, or -1 on error
◆ BMP_getImageDataSize()
| int32_t BMP_getImageDataSize | ( |
|
) |
Get imageDataSize in bytes.
- Returns
- Returns imageDataSize, or -1 on error
◆ BMP_getDataOffset()
| int32_t BMP_getDataOffset | ( |
|
) |
Get the offset, i.e.
starting address, of the byte where the bitmap data can be found.
- Returns
- Returns dataOffset, or -1 on error
◆ BMP_getFileSize()
| int32_t BMP_getFileSize | ( |
|
) |
Get the fileSize in bytes.
- Returns
- Returns fileSize, or -1 on error
Macro Definition Documentation
◆ ECODE_BMP_BASE
| #define ECODE_BMP_BASE 0x00000000 |
BMP base error code.
◆ BMP_OK
| #define BMP_OK 0x00000000 |
Successful call.
◆ BMP_END_OF_FILE
| #define BMP_END_OF_FILE |
End of file has been reached.
◆ BMP_ERROR_IO
| #define BMP_ERROR_IO ( ECODE_BMP_BASE | 0x0001) |
General IO error.
◆ BMP_ERROR_HEADER_SIZE_MISMATCH
| #define BMP_ERROR_HEADER_SIZE_MISMATCH ( ECODE_BMP_BASE | 0x0002) |
BMP_Header size in bytes is different from BMP_HEADER_SIZE.
◆ BMP_ERROR_ENDIAN_MISMATCH
| #define BMP_ERROR_ENDIAN_MISMATCH ( ECODE_BMP_BASE | 0x0003) |
Endian mismatch.
◆ BMP_ERROR_FILE_NOT_SUPPORTED
| #define BMP_ERROR_FILE_NOT_SUPPORTED ( ECODE_BMP_BASE | 0x0004) |
BMP file is not supported.
◆ BMP_ERROR_FILE_INVALID
| #define BMP_ERROR_FILE_INVALID ( ECODE_BMP_BASE | 0x0005) |
BMP "file" is not a BMP file.
◆ BMP_ERROR_INVALID_ARGUMENT
| #define BMP_ERROR_INVALID_ARGUMENT ( ECODE_BMP_BASE | 0x0006) |
Argument passed to function is invalid.
◆ BMP_ERROR_MODULE_NOT_INITIALIZED
| #define BMP_ERROR_MODULE_NOT_INITIALIZED ( ECODE_BMP_BASE | 0x0007) |
BMP module is not initialized.
Call BMP_init()
◆ BMP_ERROR_INVALID_PALETTE_SIZE
| #define BMP_ERROR_INVALID_PALETTE_SIZE ( ECODE_BMP_BASE | 0x0008) |
Invalid palette size.
◆ BMP_ERROR_FILE_NOT_RESET
| #define BMP_ERROR_FILE_NOT_RESET ( ECODE_BMP_BASE | 0x0009) |
File not reset.
Call BMP_reset()
◆ BMP_ERROR_END_OF_FILE
| #define BMP_ERROR_END_OF_FILE ( ECODE_BMP_BASE | 0x0010) |
End of bmp file is reached.
◆ BMP_ERROR_BUFFER_TOO_SMALL
| #define BMP_ERROR_BUFFER_TOO_SMALL ( ECODE_BMP_BASE | 0x0020) |
Buffer provided is too small.
◆ BMP_ERROR_PALETTE_NOT_READ
| #define BMP_ERROR_PALETTE_NOT_READ ( ECODE_BMP_BASE | 0x0030) |
Bmp palette is not read.
◆ BMP_PALETTE_8BIT_SIZE
| #define BMP_PALETTE_8BIT_SIZE (256 * 4) |
Palette size in bytes.
◆ BMP_HEADER_SIZE
| #define BMP_HEADER_SIZE (54) |
BMP Header Size in bytes.
◆ BMP_LOCAL_CACHE_LIMIT
| #define BMP_LOCAL_CACHE_LIMIT (3) |
BMP Local cache limit.
◆ RLE8_COMPRESSION
| #define RLE8_COMPRESSION (1) |
Use RLE8 compression.
◆ NO_COMPRESSION
| #define NO_COMPRESSION (0) |
Use no compression.
◆ BMP_LOCAL_CACHE_SIZE
| #define BMP_LOCAL_CACHE_SIZE (BMP_CONFIG_LOCAL_CACHE_SIZE) |
BMP Local cache size.